I have exacly the same problem. How do you fixed it?
Hello,
It is recommended to provide full power OFF -> ON instead of CPU reset,
since system boot may get hanging because of unpredictable state of external
devices, involved in boot process.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.