iMX.6DL 5.1 CTS - Failed _ OpenSSLX509CertificateTest

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX.6DL 5.1 CTS - Failed _ OpenSSLX509CertificateTest

1,356 Views
shuyuchou
Contributor I

Hi ,

We have a CTS Test failed (   OpenSSLX509CertificateTest -- testSerialization_NoContextDeserialization)  on our  custom project .

We verify the same CTS  Test on  EV board  - " IMX6 Series SABRE for Smart Devices" and get the same problems!

Is the CTS failed Known issues  ?

Can anyone Know how to solve this problems or any suggestion?

The following are failed log on IMX6 Series SABRE for Smart Devices:

Compatibility Test Package: android.core.tests.libcore.package.conscrypt ABI: armeabi-v7a

Test

Result

Details

  1. com.android.org.conscrypt.OpenSSLX509CertificateTest
-- testSerialization_NoContextDeserializationfail
  1. junit.framework.AssertionFailedError: expected:<0> but was:<-6510615555426900571> at junit.framework.Assert.fail(Assert.java:50)

Test Enviroment :

Test case :

Compatibility Test Package: android.core.tests.libcore.package.conscrypt

  1. com.android.org.conscrypt.OpenSSLX509CertificateTest -- testSerialization_NoContextDeserialization

CTS :

     CTS 5.1_r6

Freescale :

Image: Android 5.1.1 . I.MX6 DualLite (download from www.nxp.com )

CPU : iMX6DL

EVB version : IMX6 Series SABRE for Smart Devices (SABRE for Smart Devices Reference Design|NXP )

MFG tool: L5.1.1

Thanks,

shuyu.

Labels (2)
Tags (3)
0 Kudos
Reply
3 Replies

1,011 Views
art
NXP Employee
NXP Employee

Please refer to the bottom row of the Table 5 in the attached document. It says that this is the known issue, but it was still under investigation at the moment of Lollipop 5.1.1 release. Now it seems to be fixed in the latest Marshmallow 6.0.1 release.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,011 Views
shuyuchou
Contributor I

Dear Artur,

I've  check the Table 5 of the attch doc, the table only show "Some CTS use cases may fail randomly if running the whole CTS suite."

Could you please provide the detail CTS errata list .

Many Thanks,

shuyu

pastedImage_1.png

0 Kudos
Reply

1,011 Views
art
NXP Employee
NXP Employee

As the Table 5 says, the CTS use cases fail is random. So, there is no definite errata list for this issue.

Best Regards,

Artur

0 Kudos
Reply