iMX.6 IPU Adv7611 external syncs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX.6 IPU Adv7611 external syncs

Jump to solution
2,173 Views
mdonahoe
Contributor III

I have a system on the iMX6Q using the ADV7611 configured for BT.1120 YUV4228.  Everything is working fine, however, we are having an issue when it comes to passing compliance.  One of the suggestions was to switch to using external syncs (vsync,hsync,de).  I wanted to confirm that given the pinout from the ADV7611 seen below and what I'm reading in the iMX6 reference manual, specifically the IPU Sensor Interface Signal Mapping section, that it is not possible to switch to external/gated clock mode?  The subnotes 7/8 state that syncs must be embedded in the signal.  Essentially just want to confirm that I'm interpreting this correctly. 

Thank you

pastedImage_1.png

pastedImage_3.png

pastedImage_2.png

0 Kudos
Reply
1 Solution
2,105 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Michael,

You assumption are correct with the IPU is not possible change to external/gate clock mode.

Regards

View solution in original post

0 Kudos
Reply
1 Reply
2,106 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Michael,

You assumption are correct with the IPU is not possible change to external/gate clock mode.

Regards

0 Kudos
Reply