i.mx8qm: gpio_is_valid returns -517 error in built-in device driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8qm: gpio_is_valid returns -517 error in built-in device driver

Jump to solution
6,999 Views
easternblack
Contributor II

Hello.

I have a problem with gpio on I.MX8mq. My Kernel version is 5.4.70.

I experienced making device drivers in I.MX6Q, and they worked well.

Recently I'm working on MCIMX8M-EVK, and made simple driver using GPIO, I omit details because it is really really simple driver using only one GPIO for the test.


I added new device node and pinmux to .dts, but gpio_is_valid() func returns -517 error. of course I get gpio information form .dtb by using of_get_gpio().

 

I know 517 error means probing GPIO should be deferred, but the only one way to make no error is compile driver to .ko module file. and it works very well in .ko

But I want to make it built-in one.

 

Is there any ideas that make GPIO works in built-in driver? 

0 Kudos
Reply
1 Solution
6,979 Views
jimmychan
NXP TechSupport
NXP TechSupport

Hello,

 

Add defer probe handler to wait GPIO driver probe.

 

For example :

https://community.nxp.com/t5/i-MX-Processors/CS-not-working-as-GPIO-just-native/m-p/1040037

 

Another example:

drivers/spi/spi-fsl-lpspi.c | 5 +++++

 1 file changed, 5 insertions(+)
diff --git a/drivers/spi/spi-fsl-lpspi.c b/drivers/spi/spi-fsl-lpspi.c
index f919fcd383f0..ae58853fcc2c 100644
--- a/drivers/spi/spi-fsl-lpspi.c
+++ b/drivers/spi/spi-fsl-lpspi.c
@@ -895,6 +895,11 @@ static int fsl_lpspi_probe(struct platform_device *pdev)
                        for (i = 0; i < controller->num_chipselect; i++) {
                                    int cs_gpio = of_get_named_gpio(np, "cs-gpios", i);

+                                  if (cs_gpio == -EPROBE_DEFER) {
+                                              ret = -EPROBE_DEFER;
+                                              goto out_controller_put;
+                                  }
+
                                    if (!gpio_is_valid(cs_gpio) && lpspi_platform_info)
                                                cs_gpio = lpspi_platform_info->chipselect[i];

 

Best regards,

Jimmy

View solution in original post

1 Reply
6,980 Views
jimmychan
NXP TechSupport
NXP TechSupport

Hello,

 

Add defer probe handler to wait GPIO driver probe.

 

For example :

https://community.nxp.com/t5/i-MX-Processors/CS-not-working-as-GPIO-just-native/m-p/1040037

 

Another example:

drivers/spi/spi-fsl-lpspi.c | 5 +++++

 1 file changed, 5 insertions(+)
diff --git a/drivers/spi/spi-fsl-lpspi.c b/drivers/spi/spi-fsl-lpspi.c
index f919fcd383f0..ae58853fcc2c 100644
--- a/drivers/spi/spi-fsl-lpspi.c
+++ b/drivers/spi/spi-fsl-lpspi.c
@@ -895,6 +895,11 @@ static int fsl_lpspi_probe(struct platform_device *pdev)
                        for (i = 0; i < controller->num_chipselect; i++) {
                                    int cs_gpio = of_get_named_gpio(np, "cs-gpios", i);

+                                  if (cs_gpio == -EPROBE_DEFER) {
+                                              ret = -EPROBE_DEFER;
+                                              goto out_controller_put;
+                                  }
+
                                    if (!gpio_is_valid(cs_gpio) && lpspi_platform_info)
                                                cs_gpio = lpspi_platform_info->chipselect[i];

 

Best regards,

Jimmy