Hello! I've followed the steps How-To use NAND boot on i.MX6UL EVK board but this is the result after booting with mfgtools2. I am certain the nand flash is big enough. What am I doing wrong?
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
UTP: received command '$ flash_erase /dev/mtd0 0 0'
UTP: executing "flash_erase /dev/mtd0 0 0"
Erasing 2048 Kibyte @ b200000 -- 4 % complete flash_erase: Skipping bad block a
t 0b400000
flash_erase: Skipping bad block at 0b600000
random: nonblocking pool is initializedcomplete
Erasing 2048 Kibyte @ ff600000 -- 99 % complete flash_erase: Skipping bad block
at ff800000
flash_erase: Skipping bad block at ffa00000
flash_erase: Skipping bad block at ffc00000
flash_erase: Skipping bad block at ffe00000
Erasing 2048 Kibyte @ ffe00000 -- 100utp_poll: pass returned.
% complete
UTP: sending Success to kernel for command $ flash_erase /dev/mtd0 0 0.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 $FILE
'
UTP: executing "kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 $FILE"
MTD CONFIG:
chip_0_device_path = "/dev/mtd0"
chip_1_device_path = "(null)"
search_exponent = 2
data_setup_time = 80
data_hold_time = 60
address_setup_time = 25
data_sample_time = 6
row_address_size = 3
column_address_size = 2
read_command_code1 = 0
read_command_code2 = 48
boot_stream_major_version = 1
boot_stream_minor_version = 0
boot_stream_sub_version = 0
ncb_version = 3
boot_stream_1_address = 0
boot_stream_2_address = 0
-- We add the 1k-padding to the uboot.
.tmp_kobs_ng: verifying using key '00000000000000000000000000000000'
.tmp_kobs_ng: is a valid bootstream for key '00000000000000000000000000000000'
mtd: opening: "/dev/mtd0"
NFC geometry :
ECC Strength : 40
Page Size in Bytes : 8936
Metadata size : 10
ECC Chunk Size in byte : 1024
ECC Chunk count : 8
Block Mark Byte Offset : 7692
Block Mark Bit Offset : 0
====================================================
mtd: opened '/dev/mtd0' - '(null)'
mtd: mtd size too small
mtd_init failed!
UTP: sending Non-success to kernel for command $ kobs-ng init -x -v --chip_0_dev
ice_path=/dev/mtd0 $FILE.
utp_poll: exit with status 1280
已解决! 转到解答。
I've fixed the issue by applying these modifications
Commit: 2580a2a7e719ee6bf20d8d6bcbe0c01a74cd2d54 - uboot (git) - OSDN
and then recompiling u-boot like in the instructions in my original post.
By the way, to recompile you need to run `make' a little differently, like this
cd fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi-
I've fixed the issue by applying these modifications
Commit: 2580a2a7e719ee6bf20d8d6bcbe0c01a74cd2d54 - uboot (git) - OSDN
and then recompiling u-boot like in the instructions in my original post.
By the way, to recompile you need to run `make' a little differently, like this
cd fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi-