Hi i am noob, and I want to start working with i.mx6sx. but do not understand how to create a program and load it into linux to run from the cortex m4. exists a guide for dummies? hehe
My intention is to s programming and debug always from linux or from eclipse IDE as exposes in this document:
but I can not find a document same Solox
can you help
PD sorry for my bad English
Hi perales
suggest to try attached examples and use link below
Integrating Processor Expert for i.MX and ARM GCC with Eclipse
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Any UART example code (imx6sx) for ARM C compiler not for arm gcc compiler.
If anyone have, please update to me,
Regards,
Raghavendra
Email:raaguks@gmail.com
Hi,
I have used A9_launch_m4 example and able to run the code if I flash this code to SD card on imx6 solox SABRE development board.
But when I tried to flash this code to QSPI NOR flash memory using manufacturing tool, I did not see any output on UART.
Please refer the attached files that I am using with manufacturing tool.
Can you please tell me if I need to change the sources(.c or .h files) or the manufacturing tool files (ini or ucl2 files) to make this example to work with QSPI memory?
Hi igorpadykov Thanks for reply
but this document explains how to program the A9 to bare metal, explains nothing M4 cortex.
I want to know how to make a program for M4 cortex and how to to load and run it from linux embedded.
you can create a .hex and run it from ssd?
MX6SX m4 hello world uart2 is example for M4 cortex.
Sorry igorpadykov
I'm sorry but I find that in Integrating Processor Expert for i.MX and ARM GCC with Eclipse
also:
i.mx6 soloX is unsupported :smileyconfused:, where is the hello world example in cortex m4, Thanks for helping me :smileyhappy:
It is good news,but still need to be sold MMPF0200F6 :smileywink: