i.Mx audio interface by ESAI.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.Mx audio interface by ESAI.

跳至解决方案
4,959 次查看
diegoferraiuolo
Contributor I

Hello everybody,

I'm new to the community and I have a question about audio interface of DeltaSigma converters with i.MX6 processor.

For my application, I need the following configuration, that should work in Synchronous mode:

- N°3  I2S output lines

- N°2 I2S input lines

to interace with the  i.MX6 Audio Section.

Is it possible to achiev this goal by ESAI interface?

If i.MX6 should be the Master, what i.MX6 line must be used as Master Clock?

Thank you in advance for you reply.

Best Regards,

Diego Ferraiuolo

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Diego

I think your connections (i.MX6 as Master with

Synchronous Mode) are right.

~igor

在原帖中查看解决方案

0 项奖励
回复
16 回复数
3,690 次查看
chuanmunei
Contributor I

Hi Every one,

May I seek yours help to share below is correct connection for ESAI/TDM interface for audio path

I have connect this to NXP DSP IC

The BGA pad number/name all is under GPIO for IMX6

ESAI.jpg

regards

Mun Ei

0 项奖励
回复
3,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi diego

I think this is possible. For ESAI signals please look at

Table 25-1. ESAI External Signals IMX6DQRM

example connections: SCH-26662_e.pdf p.5

i.MX6_SABRE_AI_DESIGNFILES :

bare metal software examples

i.MX 6Series Platform SDK : Bare-metal SDK

iMX6_Firmware_Guide.pdf  sect.9.1 ESAI overview

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,690 次查看
diegoferraiuolo
Contributor I

Dear Igor,

thank you so much for your prompt and clear suggestions.

I would like to ask you, please, something else:

-Is it possible to connect,in the same way the ESAI CODEC is connected, separate CODECS and DACS?

I ask you because I would like to use CODEC from AKM like the AK4621 with a higher Dynamic Range (in this case 115dB).

In my application, for handling the N°3 I2S Output Lines and the N°2 I2S Input LinesI would use 2 Codecs (AK4621) and one DAC (AAK4382).

-The Master Clock, if generated internally, should be passed in Input to the i.MX6 processor too?

Are these pins CLK2_N and CLK2_P?

-If pins CLK2_N and CLK2_P are routed out of the System On Module, is it better to use the Master Clock

internally generated from i.MX6?

Thank you again.

Best Regards,

Diego

0 项奖励
回复
3,690 次查看
sinanakman
Senior Contributor III

Hi Diego

I had worked on a design for a client where we had 3 codecs

connected to ESAI ports. We used two separate set of ESAI_SCKR,

ESAI_FSR, ESAI_HCKR and ESAI_RXD/TXD. We used ADIO_PLL

based generated clock according to that Clock Generator Functional

Block Diagram Igor has referred to. Unfortunately I don't have access

to this design any more but hopefully this info will be of some help to you.

Regards

Sinan Akman

3,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Diego

ESAI has independent (asynchronous mode) or shared (synchronous mode)

transmitter and receiver sections, up to six transmitters and four receivers

with TX2_RX3, TX3_RX2, TX4_RX1, and TX5_RX0 pins shared by transmitters

2 to 5 and receivers 0 to 3.

Synchronous or asynchronous, that is, the transmitter and receiver sections

may use common clock and synchronization signals (synchronous operating mode),

or they may have their own separate clock and sync signals (asynchronous operating mode).

Regarding "Master Clock", suggest to look at Table 25-2 ., Table 25-3 IMX6DQRM

Figure 25-32. ESAI Clock Generator Functional Block Diagram

ESAI system clock, (esai_clk_root or EXTAL) can be outputted on CLKO pins with register

CCM_CCOSR , sect.18.6.21 CCM Clock Output Source Register (CCM_CCOSR) IMX6DQRM

I do not think that CLK2_N and CLK2_P can be used as master clock, its options are given in

LVDS2_CLK_SEL, sect.50.7.6 Miscellaneous Register 1 (PMU_MISC1n).

~igor

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Dear Igor,

thank you for your reply.

You are very kind and very helpful.

So I understand that I can use separate Codecs and Dacs,

but if all of them have to operate in synchronous mode,

should I use SCKR, FSR for the receiver section (ADC)

and SCKT, FST for the transmitter section (DAC), or  have I  to use only

two of them?

I ask you because in the standard Codecs, a DAC and an ADC are on the same Chip,

but there is only 1 SCK line, 1 FS line, 1 MCLK line in addition to the SDI and SDO lines. 

For the system clock (Master Clock) I understand I have to select

CLKO pins  by register CCM_CCOSR. Do you refer to CCM_CLKO1 and CCM_CLKO2?

Which pin should be used as Master Clock?

Before I told you about pins CLK2_N and CLK2_P,

as I looked to them at page 7 of the schematic sch-27767_a_x3.pdf

in the directory SABRE-AI_DualLite_CPUcard.

How it is used the Audio Oscillator ?

Thank you very much.

Best Regards.

Diego

0 项奖励
回复
3,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Diego

for connections one can look at Sabre-AI CS42888 codec, it also has

DAC and an ADC are on the same chip

CS42888 SCH-26662 p.5  i.MX6_SABRE_AI_DESIGNFILES 

ESAI system clock, (esai_clk_root or EXTAL) can be outputted on CLKO2,

selection of CLKO2_SEL.

Regarding "Audio Oscillator", Y1 is used for external

ESAI_SSI_EXT1_CLK, not for i.MX6.

~igor

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Hi Igor,

I have looked at the SCH-2662_e.pdf page 5.

The ESAI CODEC has 2 sections:

one for ADC and it uses the following signals :ESAI_SCKR, ESAI_FSR, RX0, RX1

and one for DAC where the following signals are involved: ESAI_SCKT, ESAI_FST, TX0,TX1,TX2,TX3

I think it works in Asynchronous mode. Am I wrong?

Or if it is working in Synchronous Mode SCKT=SCKR and FST=FSR?


If I have a standard I2S Codec with an ADC and a DAC and only 3 clock lines, i.e. 1xSCK 1xFS and 1x MCLK,

and if I have to work in Synchronous Mode and the  i.MX6 as Master,

should I use for that signal lines

SCKT for SCK

FST for FS

CLKO2 for MCLK

to drive my CODEC Clock Lines?

Thank you so much!!

Diego.

Standard I2S Codec.png

0 项奖励
回复
3,691 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Diego

I think your connections (i.MX6 as Master with

Synchronous Mode) are right.

~igor

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Hi Igor,

Thank you!

If I should want the i.MX6 work as SLAVE in Synchronous Mode,

how should I input the external Master Clock to the i.MX6?

Thenk you in advance for your help.

Diego.

0 项奖励
回复
3,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Diego

there is no way to input external master clock as clocks

Fsys = ipg_clk_esai, EXTAL=esai_clk_root

generated internally, shown on Table 25-3 IMX6DQRM

Figure 25-32. ESAI Clock Generator Functional Block Diagram.

~igor

~igor

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Hi Igor,

I have a doubt.

Ok, Fsys = ipg_clk_esai, EXTAL=esai_clk_root are generated internally,

and they are the source clocks for the ESAI Clock Generator (Figure 25-32).

At page 1231 of IMX6DQRM you can read:

25.2.11 High Frequency Clock for Transmitter

.................................................................................

In the synchronous mode (SYN=1), it operates as the high frequency clock input or output used by all enabled transmitters and

receivers.

.................................................................................

When programmed as output it can serve as a high frequency sample clock (to external DACs

for example) or as an additional system clock (see Table 25-3).

So it seems that HCKT should be used as Master Clock for the Codecs.

HCKT should be the ESAI_TX_HF_CLK available to the pin GPIO_4 in mode ALT0.

Am I wrong? What do you think about?

I understand that I can output the ESAI System Clock (esai_clk_root or EXTAL) on CLKO pins with register CCM_CCOSR,

but I have the doubt that the ESAI System Clock (esai_clk_root or EXTAL) is the MCLK to be passed to the CODECS.

Please, let me understand.

Thank you, again.

Best Regards,

Diego

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Hi Igor,

have you some suggestion?

Thank you in advance.

Best Regards,

Diego.

0 项奖励
回复
3,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Diego.

answer depends on what do you mean by

"Master Clock for the Codecs". Actually

Figure 25-32. ESAI Clock Generator Functional Block Diagram

shows all clock generation.

Best regards

igor

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Dear Igor,

I mean the MCLK signal of the clock.

Thank you in advance.

Best Regards,

Diego

0 项奖励
回复
3,690 次查看
diegoferraiuolo
Contributor I

Sorry, the MCLK signal of the codec.

Best Regards,

Diego

0 项奖励
回复