i.MX8X h.264 encoder bit rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8X h.264 encoder bit rate

跳至解决方案
1,162 次查看
ko-hey
Senior Contributor II

Hi all,

I have a question about H.264 encoder in i.MX8X.

According to the reference manual(Table 15-8) of i.MX8MMini, the bit rate is as below.

Minimum: 10kbps
Maximum: 40 Mbps at 1080p 60 fps

How about is it in i.MX8X ?

Ko-hey

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,083 次查看
joanxie
NXP TechSupport
NXP TechSupport

for imx8X encoder which can support up to 1080@30 fps, should be 20M bps max

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,084 次查看
joanxie
NXP TechSupport
NXP TechSupport

for imx8X encoder which can support up to 1080@30 fps, should be 20M bps max

0 项奖励
回复
1,083 次查看
ko-hey
Senior Contributor II

Hi joanxie‌,

Thank you for reply.

How about min data ? Do you have it ?

Ko-hey

0 项奖励
回复
1,083 次查看
joanxie
NXP TechSupport
NXP TechSupport

not yet, sorry

0 项奖励
回复