i.MX8X h.264 encoder bit rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8X h.264 encoder bit rate

ソリューションへジャンプ
1,055件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

I have a question about H.264 encoder in i.MX8X.

According to the reference manual(Table 15-8) of i.MX8MMini, the bit rate is as below.

Minimum: 10kbps
Maximum: 40 Mbps at 1080p 60 fps

How about is it in i.MX8X ?

Ko-hey

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
976件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx8X encoder which can support up to 1080@30 fps, should be 20M bps max

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
977件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx8X encoder which can support up to 1080@30 fps, should be 20M bps max

0 件の賞賛
返信
976件の閲覧回数
ko-hey
Senior Contributor II

Hi joanxie‌,

Thank you for reply.

How about min data ? Do you have it ?

Ko-hey

0 件の賞賛
返信
976件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

not yet, sorry

0 件の賞賛
返信