Hi,
I am using i.MX8M Mini processor (MIMX8MM4CVTKZAA) in one project having industrial surveillance application.
In datasheet, i am not able to identify behavior of ENET0_TD2 pin in RMII and RGMII mode. There may be some typo error i think (not sure about this). Refer attachment.
For your information, we want to use RMII mode.
As per my understanding, for RMII mode, this pin has two options; one for generating 50MHz clock and second for receiving 50MHz clock. And these two options are software configurable. Please confirm if i am right. If not, please help me to understand this.
Thanks in advance,
Nikhil
@nikz1402
Hello,
Your understanding is correct - ENET0_TD2 pin in RMII is used as reference clock,
input or output, depending on IOMUXC_GPR_GPR1.
Regards,
Yuri.
Hi! Did you manage to get that RMII output clock working? I need the same setup, but m ENET1_TD2 pad outputs 125 MHz, and only after I manually set bit13 in IOMUXC_GPR_GPR1 at runtime.
Any luck?
Cheers,
Mateusz
Hi,
I managed to get 50MHz RMII clock output from ENET_TD2 (Processor pin# AG25) pad.
Please check your schematic connection once or share schematic pdf here so that i can check.
If your schematic is okay, then there must be something missing/misinterpreted in code.
Regards,
Nikhil
Hi Nikhil,
I got my imx8mm on a SODIMM module (that one). Vendor does not provide schematic for it, but specified that certain sodimm pin is directly connected to AG25 procesor pad. And I have that pin connected to XI input of my PHY chip. There is not much more to it. Could you share a piece of your device tree with FEC relate pin configuration?
fsl,pins = <
MX8MM_IOMUXC_ENET_ ...
...
>;
And the fragment that descibes FEC config itself
fec1: ethernet@30be0000 {
compatible = "fsl,imx8mm-fec", "fsl,imx8mq-fec", "fsl,imx6sx-fec";
......
}
Have a nice day!
Mateusz