I've been trying to perform the EFI Capsule update procedure as detailed in sect.4.8 Arm SystemReady-IR i.MX Linux User’s Guide but haven't been able to get it to work. I also found the attached document with slightly different instructions but those don't seem to work either.
To generate the capsule, I'm using the capsule.its and the procedure from one of the "See Also" links in the second document: https://git.linaro.org/people/paul.liu/systemready/build-scripts.git/tree/docs/iotgateimx8_capsule_u...
However, the process fails with the below error:
u-boot=> efidebug capsule update -v ${loadaddr}
Capsule guid: 6dcbd5ed-e82d-4c44-bda1-7194199ad92a
Capsule flags: 0x10000
Capsule header size: 0x1c
Capsule image size: 0x361da8
Cannot handle a capsule at 0000000040480000u-boot=>
u-boot=>
Are there any updated instructions and capsule.its/capsule.bin files I can test this with?
Solved! Go to Solution.
Hi,
We were able to get this to work after tweaking the procedure to copy the capsule to the EFI System partition instead of the BOOT partition. The working procedure is as follows:
u-boot=> env set dfu_alt_info "mmc 1=1 raw 0x42 0x2000"
u-boot=> efidebug boot add 0 Boot0000 mmc 1:1 capsule1.bin;efidebug boot next 0
u-boot=> setenv -e -nv -bs -rt -v OsIndications =0x04
u-boot=> efidebug capsule disk-update /*at this point the bootloader is update*/
u-boot=> savee
u-boot=> reset
After the reset, the capsule1.bin file is deleted and the board should boot with the new bootloader
Hi,
We were able to get this to work after tweaking the procedure to copy the capsule to the EFI System partition instead of the BOOT partition. The working procedure is as follows:
u-boot=> env set dfu_alt_info "mmc 1=1 raw 0x42 0x2000"
u-boot=> efidebug boot add 0 Boot0000 mmc 1:1 capsule1.bin;efidebug boot next 0
u-boot=> setenv -e -nv -bs -rt -v OsIndications =0x04
u-boot=> efidebug capsule disk-update /*at this point the bootloader is update*/
u-boot=> savee
u-boot=> reset
After the reset, the capsule1.bin file is deleted and the board should boot with the new bootloader
Hello,
Please try by using below command in u-boot to generate the capsule image
./tools/mkeficapsule --raw flash.bin --index 1 capsule1.bin
Best regards,
Aldo.
Hi Aldo,
I just had some success with the"--raw" option in mkeficapsule you suggested. The issue seemed to be a wrong offset and mmcpart values when setting up the dfu_alt_info variable, in addition to a reset needed to initialize EFI System Partition (detailed in another post).
Now, the capsule update works through the "efidebug capsule update" command, as well as the CapsuleApp.efi in the ACS image. However, the procedure mentioned in the i.MX Linux User's guide (Section 4.8.2) still doesn't seem to work for us. U-Boot simply ignores the capsule after the reset and we don't see any indication of an update.
I'd appreciate it if you could provide any suggestions about what could be causing issues with automatic update (using "efidebug capsule disk-update"), while the manual update ("efidebug capsule update"/CapsuleApp.efi) seems to work fine.
Hello,
Got it, then please try the following:
u-boot=> env set dfu_alt_info "mmc 2=1 raw 0 0x2000 mmcpart 1"
u-boot=> efidebug boot add 0 Boot0000 mmc 2:1 capsule1.bin
u-boot=> efidebug boot next 0
u-boot=> setenv -e -nv -bs -rt -v OsIndications =0x04
u-boot=> efidebug capsule disk-update
u-boot=> reset
Best regards,
Aldo.
Hi Aldo,
Thanks, the update doesn't seem to work on the EVK after running these commands:
U-Boot SPL 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC2
NOTICE: BL31: v2.4(release):lf-5.10.52-2.1.0-rc1-39-gbb4957067
NOTICE: BL31: Built : 04:45:39, Sep 8 2021
U-Boot 2021.04-lf_v2021.04+g1c0116f3da (Sep 06 2021 - 08:48:23 +0000)CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 39C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... OK
[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22
In: serial
Out: serial
Err: serial
SEC0: RNG instantiatedBuildInfo:
- ATF bb49570switch to partitions #0, OK
mmc2(part 0) is current device
flash target is MMC:2
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
starting USB...
Bus usb@32e40000: Port not available.
USB is stopped. Please issue 'usb start' first.
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
51015 bytes read in 4 ms (12.2 MiB/s)
Scanning disk mmc@30b50000.blk...
Scanning disk mmc@30b60000.blk...
Found 5 disks
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
Remove /soc@0/bus@32c00000/usb@32e40000:extcon
Remove /soc@0/bus@30800000/ethernet@30be0000:phy-reset-gpios
Not a PE-COFF file
Loading Boot0000 'Boot0000' failed
Loading from BootNext failed, falling back to BootOrder
BootOrder not defined
EFI boot manager: Cannot load any image
Found EFI removable media binary efi/boot/bootaa64.efi
647168 bytes read in 10 ms (61.7 MiB/s)
Remove /soc@0/bus@32c00000/usb@32e40000:extcon
Remove /soc@0/bus@30800000/ethernet@30be0000:phy-reset-gpios
Booting /efi\boot\bootaa64.efi
Welcome to GRUB!
Do you know what could be causing the BootNext failure and if there are any other indications/messages we should expect in the bootlog when the disk-update is working correctly?
I'd also appreciate if you could provide us a capsule1.bin file (if you have a working one). That might help rule out any setup issues.
Thanks & Regards,
Rohit
Thanks Aldo!
The capsule update using the below command seems to work. However, the boot output doesn't seem to be any different, proving that the update went through. Also, it seems to corrupt the bootloader and the EVK doesn't get past the initial boot.
Here's the procedure I'm following on the EVK:
./uuu.exe -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk
./tools/mkeficapsule --raw imx-boot-imx8mmevk-sd.bin-flash_evk --index 1 capsule1.bin
env set dfu_alt_info "mmc 1=1 raw 0x42 0x2000"
setenv -e -nv -bs -rt -v OsIndications =0x04
fatload mmc 1:1 ${loadaddr} capsule1.bin
efidebug capsule update -v ${loadaddr}
#u-boot=> efidebug capsule update -v ${loadaddr}
Capsule guid: 6dcbd5ed-e82d-4c44-bda1-7194199ad92a
Capsule flags: 0x10000
Capsule header size: 0x1c
Capsule image size: 0x362f7c
#u-boot=>
u-boot=> reset
However, the bootlog looks exactly the same and "version" command doesn't show that the version has been updated. Do you know what I could be missing in the procedure to cause the update to be ignored?