i.MX8 ethernet cannot config static ip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8 ethernet cannot config static ip

1,564 次查看
rudolphhsueh
Contributor III

Hi NXP,

       I test the Ethernet function with android 13 on i.MX8 pluse evk. I found a problem about static ip. I cannot config the static ip after I had changed thet ethernet config dialog. Could you have any idea to solve this issue? Thanks.

0 项奖励
回复
10 回复数

1,552 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board and eth port are you using?

0 项奖励
回复

1,548 次查看
rudolphhsueh
Contributor III

Hi b45499,

      I use the prebuilt image to test the ethernet function on the 8MPLUS-BB. The OS build number is evk_8mp:13/TP1A.221005.002/bamboo02082040:userdebug/dev-keys. I check the eth port with
DHCP and it is work. Thanks.

1,541 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news it works now

0 项奖励
回复

1,476 次查看
rudolphhsueh
Contributor III

Hi b45499,

       Could you have any update for this issue?  I check the android 13 BSP of NXP. I found that the commit message(aee85dbd447c1752154bd9ccff8ad44a85b41603) like below

this patch can get ethernet config, but if we manually config the ethernet from the dialog,
fail to update the IpConfig, due to updateConfiguration seems only work on an automotive
device, I will try to use another way to fix it later.

Is the issue solved now?

thanks.

0 项奖励
回复

1,468 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

"

this patch can get ethernet config, but if we manually config the ethernet from the dialog,
fail to update the IpConfig, due to updateConfiguration seems only work on an automotive
device, I will try to use another way to fix it later.

"

What is the patch you mentioned? Could you share us the link?

0 项奖励
回复

1,339 次查看
rudolphhsueh
Contributor III

Hi NXP,

      Do you have any idea for this issue? thanks.

0 项奖励
回复

1,463 次查看
rudolphhsueh
Contributor III

Hi NXP,

          This information I get in the i.MX8 BSP. 

imx8_bsp.png

I cannot get new update to fix this issue after I run command "repo sync" for this BSP. 

Is the issue solved?

0 项奖励
回复

1,337 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you met some error messages when you download the source code?

0 项奖励
回复

1,333 次查看
rudolphhsueh
Contributor III

Hi NXP,

       No, I think that I downloaded BSP successfully. Below is my download log.

IMX8_T_BSP/android_build$ repo sync
remote: Enumerating objects: 8, done.
remote: Counting objects: 100% (8/8), done.
remote: Compressing objects: 100% (4/4), done.
remote: Total 8 (delta 4), reused 8 (delta 4), pack-reused 0
Unpacking objects: 100% (8/8), 14.47 KiB | 871.00 KiB/s, done.
project .repo/manifests/
Updating 4c3bb9d..4af837e
Fast-forward

Fetching: 100% (1137/1137), done in 18m33.668s
Checking out: 100% (1137/1137), done in 9m11.914s
repo sync has finished successfully.

       

0 项奖励
回复

1,536 次查看
rudolphhsueh
Contributor III

Hi b45499,

      We still cannot use settings->ethernet config to set static IP on i.MX8 plus. Could you give as the patch to fix this issue? thanks.

0 项奖励
回复