i.MX8 LPDDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 LPDDR4

762 Views
santosh_t
Contributor I

Hello,

We are using MIMX8MM3CVTKZAA in our design. In the EVK file of i.MX8 (SPF-31399), referring to DDR section,  all the lines of Channel A of LPDDR4 is connected to Channel B of processor. For example pin H4(CS0_A) of LPDDR4 is connected to V4(CS0_B) of processor. Is it intentional? What is the reason behind this?

Thanks & Regards,

Santosh Tuppad

Labels (1)
0 Kudos
Reply
1 Reply

661 Views
igorpadykov
NXP Employee
NXP Employee

Hi SANTOSH 

both channels are equal, so seems change was made due to board routing convenience.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply