i.MX7 PCIe clock requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7 PCIe clock requirements

1,080件の閲覧回数
ulrichschmidt
Contributor I

Dear NXP i.MX Community,

in order pass the PCIe Gen2 compliance test for i.MX6, NXP recommends an external clock. 

What about the i.MX7? Does it share the same PCIe IP? Will the internal be sufficient and what is NXP recommending? 

„PCIe reference clock solution which provided by CLKx_N/P of i.MX6 chip can't pass PCIe Gen2 compliance test.  Recommend using external PCIe 2.0/3.0 clock generator with 2 HCSL outputs solution. One clock channel connect to i.MX6 as a reference input, please click Ref14 for reference circuit. Another clock channel should connect to PCIe connector, please contact generator vendor for detailed design guide.“

 

Best regards,

Uli 

ラベル(1)
0 件の賞賛
返信
1 返信

746件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  From Table 11 (PCIE recommendations) of "Hardware Development Guide for i.MX7Dual " :

"i.MX differential clock is not compliance with PCIe standard. NXP recommends including an external clock
source that meets the PCIe jitter specification untils the i.MX 7DS PCIe jitter compliance can be assessed."

http://www.nxp.com/assets/documents/data/en/user-guides/IMX7DSHDG.pdf 

Regards,

Yuri.

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信