High Assurance Boot fails on i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

High Assurance Boot fails on i.MX6ULL

417 Views
jsopenrb
Contributor II

Using the same fuse settings and the same signed u-boot binary we can get High Assurance Boot to work on i.MX6UL but not on the i.MX6ULL. Are there any changes concerning HAB on i.MX6ULL? CPU fails to boot once SEC_CONFIG[1] fuse is blown.

0 Kudos
1 Reply

318 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Sorry, but the information you are requesting is treated as confidential info at this time and requires

a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway,

this requires to be handled as a Service Request. 

https://community.nxp.com/docs/DOC-329745 

Regards,

Yuri.

0 Kudos