i.MX7 LCD Pinout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 LCD Pinout

Jump to solution
971 Views
oneil
Contributor II

I am looking at Table 13-3 in the i.MX7 DRM:

oneil_0-1676411591609.png

I would like to use 18-bit DOTCLK mode to interface with an RGB display. I am noticing that there is no color associated with the different LCD_DATAn signals. Is this because the pinout with respect to the pixel color can be arbitrarily defined? If not, which three groups of six pins correspond to R, G, and B?

 

Thanks!

 

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
958 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @oneil,

I hope you are doing well.

Please see the 18Bit LCD connections below:

LCD_DATA[17:12] = R[5:0]

LCD_DATA[11:6] = G[5:0]

LCD_DATA[5:0] = B[5:0]

Thanks & Regards,
Ritesh M Patel

View solution in original post

3 Replies
959 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @oneil,

I hope you are doing well.

Please see the 18Bit LCD connections below:

LCD_DATA[17:12] = R[5:0]

LCD_DATA[11:6] = G[5:0]

LCD_DATA[5:0] = B[5:0]

Thanks & Regards,
Ritesh M Patel

80 Views
Bela1
Contributor III

Dear riteshmpatel,

I have the same question, but with 24 bit LCD interface.

Shall I estimate, that the signals are as follows here:

LCD_DATA[00-07] = B[0-7]

LCD_DATA[08-15]=G[0-7]

LCD_DATA[16-23]=R[0-7] ?

I mean LCD_DATA[00] = B0, LCD_DATA[01]= B1, .... and LCD_DATA[22]=R6, LCD_DATA23=R7, correspondingly. Am I correct?

Where can I find a concrete declaration of these signals in the documentation? I cannot find it either in the datasheet nor in the reference manual.

0 Kudos
Reply
953 Views
oneil
Contributor II
Thank you Ritesh, this is exactly what I was looking for.
0 Kudos
Reply