i.MX6q Boot fuse settings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6q Boot fuse settings

664 次查看
shajinas
Contributor I

Hello Nxp Team,

I'm working on a custom platform based out of the i.mx6q Sabresd platform. The software running on the custom platform is based out of Android Pie(P9.0.0_2.2.0-ga) from NXP.

The custom platform was designed to select the boot device based on the boot fuse settings. The BOOT_MODE0 & BOOT_MODE1 are set to 00. I believe the Boot ROM code will decode the value present in the BOOT_CFG1(0x21BC450), BOOT_CFG2(0x21BC460) and BOOT_CFG3(0x21BC470) registers and subsequently look for the u-boot loader on the storage medium.

I was playing around with these registers to set the boot device as the onboard eMMC . I've updated the register (0x21BC450) and (0x21BC460) through the fuse prog commands present in the bootloader. However I was not successful in booting out of eMMC also unable to revert back to default settings.

Please find the steps below which i have carried out

1) Default Value of the BOOT_CFG1 register value before start of the experiment

0x21BC450 = 0x18000030 // Boot from SPI NOR flash

0x21BC460 = 0x00000010 // BT_FUSE_SEL select

U-Boot # md 0x021BC450

021bc450: 18000030 18000030 18000030 18000030

021bc460: 00000010 00000010 00000010 00000010

 

2) Updating the register values

U-Boot # fuse prog -y 0 5 0x00005860

U-Boot # fuse prog -y 0 6 0x00000010

U-Boot # md 0x021BC450

021bc450: 18005870 18005870 18005870 18005870

021bc460: 00000010 00000010 00000010 00000010

 

3) I tried to revert back to the original settings, But unfortunately I was not successful in the process.

U-Boot # fuse prog -y 0 5 0x18000030

U-Boot # fuse prog -y 0 6 0x00000010

U-Boot # md  0x21BC450

021bc450: 18005870 18005870 18005870 18005870

021bc460: 00000010 00000010 00000010 00000010

 

Can you let me know where I went wrong in the process?

It would be really helpful if you can provide pointers on how to revert back to the default settings.

 

Thanks for your time.

 

Thanks

Shajin

标签 (1)
0 项奖励
回复
1 回复

649 次查看
Yuri
NXP Employee
NXP Employee

@shajinas 
Hello,

    It is highly recommended to try first GPIO boot overrides in order to check boot settings,
since the fuses can be burned only once.

Regards,
Yuri.

0 项奖励
回复