I am using the Variscite VAR-SOM-6UL with a i.MX6ULL processor on the Concerto Board.
Due to some conflicting pads with the project I'm working on, I switching the pin mux from
MX6UL_PAD_CSI_PIXCLK__I2C1_SCL 0x4001b8b0
MX6UL_PAD_CSI_MCLK__I2C1_SDA 0x4001b8b0
to
MX6UL_PAD_UART4_TX_DATA__I2C1_SCL 0x4001b8b0
MX6UL_PAD_UART4_RX_DATA__I2C1_SDA 0x4001b8b0
This caused it to completely stop working, not being able to communicate to anything thru I2C1.
Is there something I am missing here?
Hi @AndromedaBell,
I hope you are doing well.
The Pad configuration for the I2C1 signal seems correct.
Please cross-check that UART4 pads are not muxed for any other signal in the device tree
and i2c1 node contains status = "okay".
Thanks & Regards,
Ritesh M Patel