All,
I see in figure 10-3 of the Hardware Reference manual CLK1, CLK2 input into the clock block multiplexer section as well as the main 24MHZ oscillator. I see that there are pins CLK1_N/CLK1_P differential inputs for CLK1, but I cannot seem to find any reference to input CLK2 in the IO ALT#. There is a bunch of references to the CLK1/CLK2 outputs, just not the input CLK2.
I want to feed known audio Master Clocks into CLK2 single ended, bypass the audio pll and use this clock to derive the I2S and possibly SPDIF output feeds.
Thanks,
Gordon
Solved! Go to Solution.
Both SAI_MCLK and SPDIF_EXT_CLK inputs can run at the frequencies of up to 50MHz.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
All,
Looks like a better avenue than CLK1/CLK2 as an input into the MUX, is to use the MCLK as an input to generate the I2S feed.
For the SPDIF output I can use the SPDIF_EXT_CLK input to generate the the SPDIF output feed.
Anyone know what the maximum clock rates for these two CLK inputs are?
Thanks,
Gordon
Both SAI_MCLK and SPDIF_EXT_CLK inputs can run at the frequencies of up to 50MHz.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Artur,
Thanks!
Gordon