i.MX6UL Ethernet Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL Ethernet Driver

1,143 次查看
TerryMcHenry
Contributor II

The Ethernet from Freescale states;

* The dual fec interfaces are not equivalent with enet-mac.

* Here are the differences:

*

* - fec0 supports MII & RMII modes while fec1 only supports RMII

* - fec0 acts as the 1588 time master while fec1 is slave

* - external phys can only be configured by fec0

*

* That is to say fec1 can not work independently. It only works

* when fec0 is working. The reason behind this design is that the

* second interface is added primarily for Switch mode.

*

* Because of the last point above, both phys are attached on fec

* mdio interface in board design, and need to be configured by

* fec0 mii_bus.

Does this means that 1588 timing synchronization can only be achieved from the ENET1 input?

标签 (1)
0 项奖励
回复
1 回复

669 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned comments (restrictions) relate to i.MX28 device (with hardware switch support).

As for i.MX6UL, please refer to its documentation

i.MX 6UltraLite Applications Processor|NXP

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复