I've got a custom board based around the i.MX6SoloLite EVK and am trying to build linux kernel 3.0.35 using LTIB. I have build the kernel successfully and loaded it onto the board via tftp. When I try to boot the kernel I get the following:
=> run bootcmd_mmc
mmc0(part 0) is current device
MMC read: dev # 0, block # 2048, count 8192 ... 8192 blocks read: OK
## Booting kernel from Legacy Image at 80800000 ...
Image Name: Linux-3.0.35-2666-gbdde708
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3585076 Bytes = 3.4 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ...
Then the board resets back into U-Boot. I've got a custom U-Boot build for our board that is NOT build using LTIB. Clearly the 'Load Address' and the 'Entry Point' are not correct for the i.MX6SL processor. Are these configured in LTIB? I've not been able to find where I can define this addresses. Any advice?
已解决! 转到解答。
The kernel should be generated with the correct LOADADDR:
make -j4 uImage LOADADDR=0x80008000
Also, if you use U-boot 2014.04 the default kernel type is zImage, which makes things a bit easier.
Hello FabioEstevam
Thanks for the reply.
The kernel should be generated with the correct LOADADDR:
make -j4 uImage LOADADDR=0x80008000
Is this something that is not done by LTIB? Do you know of settings in LTIB which I can modify to the LOADADDR? Or is this something that I have to do outside of LTIB? Seems odd that I would have to regenerate the uImage since LTIB generates one for me already.
Also, if you use U-boot 2014.04 the default kernel type is zImage, which makes things a bit easier.
I think an upgrade is in the future, but for now I'm stuck using the 2013.10 version.
Thanks for your help!
Hi Leo,
I *thought* I did that...
baudrate=115200
bootfile=uImage
ethact=FEC
ethaddr=12:34:56:78:9a:bc
ethprime=FEC
ipaddr=192.168.1.123
loadaddr=80800000
serverip=192.168.1.105
stderr=serial
stdin=serial
stdout=serial
Is this not what you mean?
Do you know if LTIB provides a means to override the configuration for the Load Address and Entry Point contained in the header of a uImage? If it does, can you provide some direction as to where one can find it? If not, can you provide a manual method to override these settings?
Thanks,
Kevin
It looks to me like the header on the kernel image contains the entry-point and the load-address...U-Boot appears to look these items up from the header of the image file. I'm using the uImage file created from LTIB...perhaps I need to use the zImage? I'm not completely sure the differences...
(from the u-boot-imx source code common/image.c in function image_print_contents)
printf("%sLoad Address: %08x\n", p, image_get_load(hdr));
printf("%sEntry Point: %08x\n", p, image_get_ep(hdr));
I do not see anywhere in the source that has that address hardcoded. FWIW here's my boot command for booting from mmc (all these are in environment variables):
bootargs=root=/dev/mmcblk0p1 rootwait rw max17135:pass=2,vcom=-2030000 video=mxcepdcfb:E060SCM,bpp=16
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw max17135:pass=2,vcom=-2030000 video=mxcepdcfb:E060SCM,bpp=16
bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 0;mmc read ${loadaddr} 800 2000; bootm
bootcmd=run bootcmd_mmc
**note that all of the above was from the i.MX6SoloLite EVK Linux Users Guide and I don't expect it fully work, but I do expect it to load the kernel; I expect the kernel to crash elsewhere
then while running U-Boot I type: run bootcmd.
It does appear that in the bootcmd_mmc env variable, the expression ${loadaddr} is being expanded properly because it is loading the contents of the mmc to that address.
So do you know how the header of the uImage file is generated? Is this LTIB's doing?