i.MX6QuadPlus/DualPlus DDR performance, SATA read speed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6QuadPlus/DualPlus DDR performance, SATA read speed?

898 Views
sergeydanilov
Contributor III

Hello,

Could you please post some basic DDR performance test data comparison like memory to memory copy speed for imx6 quad and imx6 quad plus.

Or may be you can just post results of LMBench for imx6 quad and imx6 quad plus?

Is there any improvement in SATA read speed (in case of fast SSD sata disk usage)

Thanks!

Labels (1)
0 Kudos
Reply
2 Replies

580 Views
niklasmolin
Senior Contributor I

Hi.

Will this performance be noticed when just running application in linux or is it mostly when using the graphic part of the processor?

Thanks

Niklas

0 Kudos
Reply

580 Views
igorpadykov
NXP Employee
NXP Employee

Hi sergeydanilov

there will be significant improvement in DDR performance, as

ERR003740,42 were fixed. I am not aware of SATA improvements.

Performance data is not available as product not yet released.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply