i.MX6QuadPlus/DualPlus DDR performance, SATA read speed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6QuadPlus/DualPlus DDR performance, SATA read speed?

847件の閲覧回数
sergeydanilov
Contributor III

Hello,

Could you please post some basic DDR performance test data comparison like memory to memory copy speed for imx6 quad and imx6 quad plus.

Or may be you can just post results of LMBench for imx6 quad and imx6 quad plus?

Is there any improvement in SATA read speed (in case of fast SSD sata disk usage)

Thanks!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

529件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

Will this performance be noticed when just running application in linux or is it mostly when using the graphic part of the processor?

Thanks

Niklas

0 件の賞賛
返信

529件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sergeydanilov

there will be significant improvement in DDR performance, as

ERR003740,42 were fixed. I am not aware of SATA improvements.

Performance data is not available as product not yet released.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信