I'm trying to decide on the display hardware to purchase for the i.MX6QP-SABRE SD.
I have read that the board is compatible with the following: MCIMX-LVDS1, MCIMX28LCD and possibly MCIMXHDMICARD.
I am currently using the on-board HDMI as my primary output.
Has anyone tried HDMI + either LVDS, LCD, HDMICARD successfully on the i.MX6QP-SABRE-SD (I believe i.MX6Q-SABRE-SD should be similar)?
My ultimate goal would be to output 2 independent displays with the GPU.
EDIT: By the way, I am using Yocto.
Any help is appreciated.
Thanks
解決済! 解決策の投稿を見る。
The thread is created by my couleague https://community.nxp.com/docs/DOC-332671 on i.MX6Q, you can take it as an reference.
Hi,
Which version BSP are you using? Our android BSP on i.MX6QP-SABRE SD support dual display.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rita,
I'm using Linux 4.1.15_2.0.1 Patch.
I understand from the Linux Release Notes that LVDS + HDMI is supported.
Just wondering what other configurations are possible and if anyone had tried them before purchasing the hardware.
Thanks
Jacob
Other display is OK, if it is not the default display support, you need to porting the screen diver to your board.
Thanks Rita,
Have decided to purchase the LVDS panel for evaluation.
Jacob