Hi
I have occur the problem that i.MX6Q have no display with prebuild image boot from eMMC.
Below are my steps:
1. Copy the following files in release_package/image_*/sabresd_6dq to your MFGTool-Dir/Profiles/MX6Q Linux
Update/OS Firmware/files/android/ directory.
eMMC/boot.img
u-boot-6q.bin and renamed it to u-boot.bin
eMMC/system.bin
eMMC/recovery.bin
2. Change the SABRE SD SW6 (boot) to 00001100 (from 1-8 bit) to enter download mode.
3. And download the images by MFGTool
4. Download sucessful.
5.Change Boot Switch (SW6) to 11100110 (from 1-8 bit) to switch the board back to eMMC boot mode.
6. Power on / reset
7. Under the U-Boot prompt, please set the following U-Boot environment variable:
I tried to boot with LVDS single display mode and boot with HDMI single display mode and boot with LVDS & HDMI dual display mode.All of these have no display.
There something wrong? BTW,when dowanloading the images it have display with 4 penguins
Please help,thanks.
Attached is the log messages
Original Attachment has been moved to: No-display-log.txt.zip
Solved! Go to Solution.
Hi,
According to your log your video mxcfb0 is not set.
Use follwoing commands at uboot promt, for HDMI display.
--> setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off video=mxcfb2:off fbmem=28M
--> saveenv
Reboot the hardware, it will give you output your HDMI dipslay.
Thanks,
Saurabh
PicusTech Software
Hi,
According to your log your video mxcfb0 is not set.
Use follwoing commands at uboot promt, for HDMI display.
--> setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off video=mxcfb2:off fbmem=28M
--> saveenv
Reboot the hardware, it will give you output your HDMI dipslay.
Thanks,
Saurabh
PicusTech Software