Dear NXP
When using imx6Q as an RC, does the use of "power-on-gpio" depend on the setting of the PCIE_WAKE pin?
If I add a pull-up resistor in PCIE_WAKE line, I do not need to use power-on-gpio,
and If there is no resistor, is it necessary to trigger the internal PCIE PHY via power-on-gpio?
Thanks & regards
heecheol.jung
解決済! 解決策の投稿を見る。
Hi heecheol
yes it is different pin and has not relation to wake-up-gpio or PCIE_WAKE,
description can be found on
Best regards
igor
Hi heecheol
could you say where did you find PCIe "power-on-gpio" in nxp linux
and linux documentation
https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...
In general PCIE_WAKE is not used, for waking functionality gpio may be used:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor
Thanks for reply
In the items below there is no 'wake-up-gpio' and there is 'power-on-gpio',
is the name changed as the kernel version is up?
[ kernel 4.9.11 ]
in drivers/pci/host/pci-imx6.c (imx6_pcie_probe method)
[ kernel 4.14.78 ]
in drivers/pci/dwc/pci-imx6.c (imx_pcie_probe method)
Thanks & regards
heecheol.jung
Hi heecheol
thanks, as decribes code it is used for enable power
imx_pcie->power_on_gpio = of_get_named_gpio(node, "power-on-gpio", 0); if (gpio_is_valid(imx_pcie->power_on_gpio)) { ret = devm_gpio_request_one(&pdev->dev, imx_pcie->power_on_gpio, GPIOF_OUT_INIT_LOW, "PCIe power enable");Best regards igor
Dear Igor
Thanks for reply
if so, is power-on-gpio and wake-up-gpio a completely different pin?
and please let me know about pull-up resistor.
Is there a problem without a pull-up resistor in the PCIE_wake line? (ex> float?)
Thanks & regards
heecheol.jung
Hi heecheol
yes it is different pin and has not relation to wake-up-gpio or PCIE_WAKE,
description can be found on
Best regards
igor