i.MX6Q Sabre Lite Kernel boot Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q Sabre Lite Kernel boot Problem

2,221 次查看
youneschalabi
Contributor III

Hi,

I'm trying to install xenomai-2.6.2.1 on the i.MX6Q Sabre Lite.

Using U-boot-mx6q-sabrelite.bin and the rootfs.ext2 from the L3.0.35_4.0.0_130424_images_MX6 directory.

The kernel used is rel_imx_3.0.15_12.03.00, and after patching it with xenomai-2.6.2.1 following these steps :

1- Applying xenomai-2.6.2.1/ksrc/arch/arm/patches/mxc/adeos-ipipe-3.0.36-arm-1.18-11-pre.patch

2- Applying xenomai-2.6.2.1/ksrc/arch/arm/patches/adeos-ipipe-3.0.36-arm-1.18-11.patch

3- Applying xenomai-2.6.2.1/ksrc/arch/arm/patches/mxc/adeos-ipipe-3.0.36-arm-1.18-11-post.patch

4- xenomai-2.6.2.1/scripts/prepare-kernel.sh --arch=arm --adeos=$xenomai_root/ksrc/arch/arm/patches/adeos-ipipe-3.0.36-arm-1.18-11.patch --linux=rel_imx_3.0.15_12.03.00

5- make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- O=$build_root/linux imx6_defconfig

6- make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- O=$build_root/linux bzImage modules

7- xenomai-2.6.2.1/configure CFLAGS="-march=armv7-a -mfpu=vfp3" FDFLAGS="-march=armv7-a -mfpu=vfp3" --build=i686-pc-linux-gnu --host=arm-none-linux-gnueabi

8- make DESTDIR=$staging_dir install

Then putting the build_root/linux/arch/arm/boot/uImage | System.map | modules.builtin |   modules.order |  Module.symvers      ==> to /media/boot

But when booting the target the kernel doesn't start and have this display :

mmc1 is current device

MMC read: dev # 1, block # 2048, count 8192 ... 8192 blocks read: OK

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-$ (3.0.15_12.03.00)

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3813344 Bytes =  3.6 MB

   Load Address: 10800000

   Entry Point:  10800000

   Verifying Checksum ... OK

   XIP Kernel Image ... OK

OK

Starting kernel ...

"Stops here"

Any help or idea is welcome

标签 (1)
0 项奖励
回复
1 回复

1,549 次查看
youneschalabi
Contributor III

Hi,

I want to install xenomai on the i.MX6Q Sabre Lite board, for this I followed differents strategies but still not able to have xenomai on the target.

     1- linux-3.5.7 vs xenomai-2.6.2.1 vs ipipe-core-3.5.7-arm-3.patch :

          Using the installation procedure for ARM from : www.xenomai.org/documentation/xenomai-2.6/html/README.INSTALL/

               The problem with this strategy is that I hadn't a rootfs to boot the target, so I took a different strategy.

                    HOW CAN I HAVE A ROOTFS TO BOOT THE TARGET WITH THE COMPILED SOURCES ?

     2- Using the L3.0.35_4.0.0_130424 Freescale Release I built LTIB and by the way a rootfs, an uImage and a u-boot.bin which work correctly on the target.

          Once having the rootfs I wanted to build the kernel patching it with xenomai and using the previous rootfs (LTIB)

               PATCHING FAILED

     3- I tried to patch the linux-3.0.35 with : adeos-ipipe-3.0.36-arm-1.18-11-pre.patch | adeos-ipipe-3.0.36-arm-1.18-11.patch | adeos-ipipe-3.0.36-arm-1.18-11-post.patch

          But I had so many rejects, that why I prefered to use the rel_imx_3.0.15_12.03.00 and it's advised in : xenomai-2.6.2.1/ksrc/arch/arm/patches/README

               Doing the same procedure as for linux-3.5.7, I had an uImage that I loaded on the µ-SD with the rootfs and u-boot either with the generated files from LTIB or the L3.0.35_4.0.0_130424_images_MX6

                    THE KERNEL LAUNCH BUT DOESN'T START :

                          mmc1 is current device

                          MMC read: dev # 1, block # 2048, count 8192 ... 8192 blocks read: OK

                          ## Booting kernel from Legacy Image at 10800000 ...

                             Image Name:   Linux-$ (3.0.15_12.03.00)

                             Image Type:   ARM Linux Kernel Image (uncompressed)

                             Data Size:    3813344 Bytes =  3.6 MB

                             Load Address: 10800000

                             Entry Point:  10800000

                             Verifying Checksum ... OK

                             XIP Kernel Image ... OK

                           OK

                           Starting kernel ...

                           "Stops here"

How can I have a rootfs that woks with a kernel patched with xenomai ? To boot the target ?

Waiting for your answers.

Best regards,

Younes

0 项奖励
回复