i.MX6Q MJPEG decoding error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q MJPEG decoding error

ソリューションへジャンプ
2,257件の閲覧回数
Tarek
Senior Contributor I

Hi,

I'm trying to decode MJPEG stream from IP camera but I'm getting VPU errors. I have enable the VPU wrapper debugging and I get this message:

The Jpeg Image must be another profile

What does this mean?

It is clear that vpu_DecStartOneFrame() is returning RETCODE_JPEG_BIT_EMPTY but I'm not sure why!


Here is the full log:

Media type image/jpeg, width=(int)640, height=(int)480 found, probability 100%

calling vpu_DecOpen() : filePlayEnable: 0 , format: 7

[INFO] bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0

calling vpu_DecGetBitstreamBuffer()

calling vpu_DecGetBitstreamBuffer()

calling vpu_DecGetBitstreamBuffer()

Wr: 0x16000000, Rd: 0x16000000, space: 3145727

calling vpu_DecUpdateBitstreamBuffer(): 41121

calling vpu_DecSetEscSeqInit(): 1

calling vpu_DecGetInitialInfo()

[INFO] The Jpeg Image must be another profile

calling vpu_DecSetEscSeqInit(): 0, interlace: 0 , errcode: 0x0

VpuSeqInit:vpu init OK: [width x heigh]=[640 x 480]

hwbuf allocator zone(462848) created

input register frame 0: (phy) Y:0x19F80000, U:0x19FCB000, V:0x19FDDC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 0: (virt) Y:0x3752B000, U:0x37576000, V:0x37588C00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 0: (phy) Y:0x19F80000, U:0x19FCB000, V:0x19FDDC00

register mv    0: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

input register frame 1: (phy) Y:0x19780000, U:0x197CB000, V:0x197DDC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 1: (virt) Y:0x3759C000, U:0x375E7000, V:0x375F9C00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 1: (phy) Y:0x19780000, U:0x197CB000, V:0x197DDC00

register mv    1: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

input register frame 2: (phy) Y:0x18580000, U:0x185CB000, V:0x185DDC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 2: (virt) Y:0x3760D000, U:0x37658000, V:0x3766AC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 2: (phy) Y:0x18580000, U:0x185CB000, V:0x185DDC00

register mv    2: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

input register frame 3: (phy) Y:0x16700000, U:0x1674B000, V:0x1675DC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 3: (virt) Y:0x3767E000, U:0x376C9000, V:0x376DBC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 3: (phy) Y:0x16700000, U:0x1674B000, V:0x1675DC00

register mv    3: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

input register frame 4: (phy) Y:0x16600000, U:0x1664B000, V:0x1665DC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 4: (virt) Y:0x376EF000, U:0x3773A000, V:0x3774CC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 4: (phy) Y:0x16600000, U:0x1664B000, V:0x1665DC00

register mv    4: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

input register frame 5: (phy) Y:0x16680000, U:0x166CB000, V:0x166DDC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 5: (virt) Y:0x37760000, U:0x377AB000, V:0x377BDC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 5: (phy) Y:0x16680000, U:0x166CB000, V:0x166DDC00

register mv    5: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

input register frame 6: (phy) Y:0x16500000, U:0x1654B000, V:0x1655DC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

input register frame 6: (virt) Y:0x377D1000, U:0x3781C000, V:0x3782EC00 , Y_TileBot: 0x0, Cb_TileBot: 0x0

vpu register frame 6: (phy) Y:0x16500000, U:0x1654B000, V:0x1655DC00

register mv    6: (phy) 0x37C52D00,    (virt)    0x2B94EEFC

calling vpu_DecRegisterFrameBuffer()

vpu_DecGiveCommand: SET_ROTATION_ANGLE: 0

vpu_DecGiveCommand: SET_MIRROR_DIRECTION: 0

vpu_DecGiveCommand: SET_ROTATOR_STRIDE: 640

vpu_DecGiveCommand: SET_ROTATOR_OUTPUT: 0

calling vpu_DecStartOneFrame(): 41121, skipmode: 0

[INFO] The Jpeg Image must be another profile

MJPG: BIT EMPTY

calling vpu_DecGetBitstreamBuffer()

Wr: 0x1600A0A1, Rd: 0x16000000, space: 3104606

vdecode.c(924): App Source Queue is full for decoder 0

calling vpu_DecUpdateBitstreamBuffer(): 41662

vpu_DecGiveCommand: SET_ROTATOR_OUTPUT: 0

calling vpu_DecStartOneFrame(): 41662, skipmode: 0

[INFO] The Jpeg Image must be another profile

MJPG: BIT EMPTY

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,806件の閲覧回数
jack_mao
NXP Employee
NXP Employee

Hi Vlandan,

    The video  container is MKV, from our release document, mkv doesn't support MJPEG, you should find *.avi or *.mp4 mjpeg file.

Jack

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,807件の閲覧回数
jack_mao
NXP Employee
NXP Employee

Hi Vlandan,

    The video  container is MKV, from our release document, mkv doesn't support MJPEG, you should find *.avi or *.mp4 mjpeg file.

Jack

0 件の賞賛
返信