i.MX6Q Android 6.0.1 HDMI re-plug issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q Android 6.0.1 HDMI re-plug issue

2,560 Views
m_c
Senior Contributor I

Customer found i.MX6Q Android 6.0.1 screen will became weird (HDMI-display-weird.jpg) and console show error message (HDMI-error-console.jpg) after plugin/out HDMI cable several times. However, this issue isn't easy to duplicate manually . So customer use another way to duplicate with below command (HDMI-error-console.jpg). Then screen will became weird and show error message same as plugin/out HDMI cable serveral times manually. If change mode back, the screen will became normal (HDMI-display-re-change.jpg), but with flick and mouse cursor lag, and error message (imx6.gralloc: FBIOPAN_DISPLAY failed: Invalid argument) still keep print.

Hardware: MCIMX6Q-SDP

Software: Android 6.0.1

cd /sys/class/graphics/fb0

echo "V:640x480p-60" > mode

logcat -c

logcat

imx6.gralloc: FBIOPAN_DISPLAY failed: Invalid argument

Labels (3)
0 Kudos
Reply
5 Replies

2,255 Views
diegoadrian
NXP Employee
NXP Employee

Hello

I apologize for the delay. 

Let me verify with my board. I will let you know if I can reproduce the error.

Best Regards,

Diego.

0 Kudos
Reply

2,255 Views
frankweng
Contributor III

Hi Diego Adrian Cuevas

Is this problem solved?

0 Kudos
Reply

2,255 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize for the delay.

Unfortunately, the problem is still not solved, I am still working on that. It seems to be a problem with a buffer overflow. Please give some time. I apologize for the inconveniences this is taking to you.

Best regards.

Diego.

0 Kudos
Reply

2,255 Views
frankweng
Contributor III

Thank you, in the trouble you have any solution informing me, thank you.

0 Kudos
Reply

2,255 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Just to inform you about the updates.

I tested also with the Android 7 version. But apparently, the commands that you are using does nothing to the Android image output. Can you please see if that version solves the problem that you have?

Best Regards,

Diego.

0 Kudos
Reply