i.MX6DL Automotie Lifetime estimatiion at 996MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DL Automotie Lifetime estimatiion at 996MHz

ソリューションへジャンプ
1,490件の閲覧回数
ko-hey
Senior Contributor II

Hi all

 

I'm finding a lifetime estimation data for i.MX6DL automotive grade at 996MHz.

Because my customer plant to use MCIMX6U6AVM10AC.

 

I have checked section 1.1.3 of AN4725 but there're no data for ARM core speed at 996MHz.

https://www.nxp.com/docs/en/application-note/AN4725.pdf

 

On the other hand, I found a similar data in section 1.1.2 of AN4724.

So I guess that NXP also has the data for i.MX6DL.

https://www.nxp.com/docs/en/application-note/AN4724.pdf

 

 

Could you provide me the data for i.MX6DL automotive for 996MHz ?

(*Reference values are acceptable, so please provide them.)

 

Ko-hey

 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,307件の閲覧回数
b36401
NXP Employee
NXP Employee

Here I attached lifetime estimation for both 792MHz and 996MHz frequences I got from Experts Team.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,308件の閲覧回数
b36401
NXP Employee
NXP Employee

Here I attached lifetime estimation for both 792MHz and 996MHz frequences I got from Experts Team.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,307件の閲覧回数
b36401
NXP Employee
NXP Employee

I am going to forward the question to our Experts Team.
However I need a case to point it in the form.
Please create a technical case:
https://community.nxp.com/thread/381898

Have a great day,
Victor

0 件の賞賛
返信
1,306件の閲覧回数
ko-hey
Senior Contributor II

Hi b36401

I made case 00143637.

Could you follow it ?

Ko-hey

0 件の賞賛
返信
1,306件の閲覧回数
ko-hey
Senior Contributor II

Could someone follow and answer this thread ?

Ko-hey

0 件の賞賛
返信