I'm using the i.MX6 SABRE MCIMX6Q-SDB out of the box the Android boots from the SC card but I need to use Yocto and I need a "core-image-base."
So, I utilized the MOST CURRENT (I think) Freescale Yocto Project User's Guide, Rev. 0, 04/2016 and successfully got a "core-image-base-imx6qsabresd.sdcard" which is an 84.0 MB file.
When I image the SD card with dd as per section 6.1 Flashing an SD card image, I can see the following:
Boot imx6qs 8.4 MB FAT - and that has the "zImage" and the "imx6q-sabresd.dtb" file(s) on /dev/sdd1
and /dev/sdd2 has the root file system.
Here is the boot :
_____________________________________________________________________________
U-Boot 2015.04imx_v2015.04_4.1.15_1.2.0_ga+gede7538 (Sep 06 2016 - 17:19:19)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 24 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
Error reading cluster
** Unable to read file zImage **
Booting from net ...
FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
_____________________________________________________________________________
Oh, yes I checked and the SW6 on the board and it is set correctly - I.MX 6 SABRE-SD boards in the Linux User's Guide, Rev. L4.1.15_1.0.0-ga, 03/2016 Table 8 -- which I expected because the Android boots from the SD card.
I REALLY NEED HELP SOLVING THIS - THANKS in ADVANCE
Hi What is the last solution for this issue.
I also experienced a similar problem and found a solution in a commit message for the u-boot project from April 2016. The text of that commit message is
mx6ul_evk does not come with a eMMC populated, so we should not
define CONFIG_SUPPORT_EMMC_BOOT as it causes SPL to not be able
to boot some brands of SD cards, such as SanDisk microSD HC - 8GB:U-Boot SPL 2016.05-rc1-28384-g108f841 (Apr 19 2016 - 11:19:11)
Trying to boot from MMC1
spl: mmc block read error
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###When CONFIG_SUPPORT_EMMC_BOOT is defined spl_boot_mode() returns
MMCSD_MODE_EMMCBOOT, so remove this option to have a reliable boot
via SD card.
This referenced a different board than I was using, but the problem was the same. The microSD card I experienced the problem with was a SanDisk 4GB.
The CONFIG_SUPPORT_EMMC_BOOT is defined in /include/configs/mx6xxxxx.h in the u-boot source and is specific to your board configuration.
Hope that helps.
Janet, we've just experienced similar pain flashing an image on two different 8GB Patriot SD cards, both yielding the same error as you:
reading zImage
Error reading cluster
After seeing your post we decided to try a 16GB Kingston and suddenly it was ok. All cards were class 10.
Hi Janet,
You could try to compare the partition table of your failed SD Cards with the working ones and check if you can recover any of them.
BTW, these days even I am encountering many faulty (inconsistent) SD cards.
Regards,
Balaji
So, from looking more at the u-boot and what "printenv" has which is above, u-boot FIRST tries to boot from the SD card, I think, but the commands are unsuccessful so then it tries the net:
So, does that mean the SD card is not correct?
WHEN I DO THINGS MANUALLY I GET
=> mmc dev 1
switch to partitions #0, OK
mmc1 is current device
COMMENT -- this seems fine to me because /dev/sdd1 was where I saw the zImage and .dtb
=> mmc rescan
=> fatload mmc 1:1 0x12000000 boot.src
reading boot.src
** Unable to read file boot.src **
COMMENT -- so here I'm in trouble !!
=> fatload mmc 1:1 0x12000000 zImage
reading zImage
Error reading cluster
** Unable to read file zImage **
COMMENT -- so here I'm in MORE Trouble !!
SO, IF I CAN SEE THE FILES ON THE SD-CARD what can cause this problem??
THANKS IN ADVANCE
I can also do:
=> mmc rescan
=> fatls mmc 1
6618968 zimage
45464 imx6q-sabresd.dtb
-- other .dtb files --
6 file(s), 0 dir(s)
=>
SO THAT LEADS ME TO BELIEVE that the "zimage" is ??? with the Error reading cluster ???
Hello,
Please check U-boot environment - if it is set properly for SD boot.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Janet,
On the terminal, when the string "Hit any key to stop autoboot:" appears, just press any key. You will be presented with a terminal. You need to enter "printenv" command. You need to pay more attention to "bootcmd" environment variable.
For further details on environment variables, you could refer to the following link:
UBootEnvVariables < DULG < DENX
Regards,
Balaji.V
Balaji,
O.K. so here is what "printenv" shows with the u-boot.
------------------------------------------------------------------------------------------------------
=> printenv
baudrate=115200
boot_fdt=try
bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimi
bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
bootdelay=1
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
emmcdev=2
epdc_waveform=epdc_splash.bin
ethact=FEC
ethaddr=00:04:9f:04:18:c2
ethprime=FEC
fdt_addr=0x18000000
fdt_file=imx6q-sabresd.dtb
fdt_high=0xffffffff
image=zImage
initrd_addr=0x12C00000
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x12000000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.re
mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}
mmcautodetect=yes
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk2p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else sete;
script=boot.scr
update_emmc_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if ${gi
update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc di
Environment size: 2678/8188 bytes
=>
---------------------------------------------------------------------------------------------------------------------------------------------------
So, being new to this, how do I get this default to booting to the SD card? I believe the variables are all ready for me so that if I booted from the "=>" prompt it might work, but I'm not sure of the syntax.
THANKS !!!