Hi all
I have a question about i.MX6 security features.
My customer have considered a CPU that it supports EVITA-Full(High).
The EVITA-Full is automotive security specification and it need some security modules.
Evita Specification ( http://www.evita-project.org )
Can i.MX6's seciruty modelus satisfy the EVITA-Full specification ?
According to the following presentation material in P45, it seems i.MX6 doesn't support EVITA-Full.
But I can not have conclusive evidence.
So please let me know.
http://cache.freescale.com/files/FTF_2015/ftf-acc-f1265.pdf?fsrch=1&sr=1&pageNum=1
Ko-hey
解決済! 解決策の投稿を見る。
Hello Ko-Hey
Yes unfortunately the i.Mx6 does not support EVITA High specification the device only achieve the EVITA Medium. You can get more details in the following link:
http://www.freescale.com/files/training/doc/dwf/DWF13_AMF_AUT_T0112_Detroit.pdf
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Ko-Hey
Yes unfortunately the i.Mx6 does not support EVITA High specification the device only achieve the EVITA Medium. You can get more details in the following link:
http://www.freescale.com/files/training/doc/dwf/DWF13_AMF_AUT_T0112_Detroit.pdf
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jaime
Thank you for your support.
Ko-hey
Hi @jamesbone ,
I would like to get the doc that you linked in this thread.
Could you share it again ?
Ko-hey