i.MX6 UL Silicon Rev 1.1 Available?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 UL Silicon Rev 1.1 Available?

ソリューションへジャンプ
1,264件の閲覧回数
durmus
Contributor IV

Hi,

We are having problems due to 24 MHz external crystal not working with Rev 1.0. Errata says the issue is fixed with Rev 1.1.

The ordering code does not differentiate Rev 1.1 from Rev 1.0 (they both have "A" at the end), only the marking on the device (1N52P for Rev 1.1 and 0N52P for Rev 1.0). So, is Rev 1.1 available and ready to be used?

Thanks.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
829件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

production target is April 29, for earlier availability

please contact local marketing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
830件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

production target is April 29, for earlier availability

please contact local marketing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信