i.MX6 UL Silicon Rev 1.1 Available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 UL Silicon Rev 1.1 Available?

Jump to solution
1,263 Views
durmus
Contributor IV

Hi,

We are having problems due to 24 MHz external crystal not working with Rev 1.0. Errata says the issue is fixed with Rev 1.1.

The ordering code does not differentiate Rev 1.1 from Rev 1.0 (they both have "A" at the end), only the marking on the device (1N52P for Rev 1.1 and 0N52P for Rev 1.0). So, is Rev 1.1 available and ready to be used?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
828 Views
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

production target is April 29, for earlier availability

please contact local marketing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
829 Views
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

production target is April 29, for earlier availability

please contact local marketing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply