i.MX6 UL Silicon Rev 1.1 Available?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 UL Silicon Rev 1.1 Available?

跳至解决方案
1,262 次查看
durmus
Contributor IV

Hi,

We are having problems due to 24 MHz external crystal not working with Rev 1.0. Errata says the issue is fixed with Rev 1.1.

The ordering code does not differentiate Rev 1.1 from Rev 1.0 (they both have "A" at the end), only the marking on the device (1N52P for Rev 1.1 and 0N52P for Rev 1.0). So, is Rev 1.1 available and ready to be used?

Thanks.

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
827 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

production target is April 29, for earlier availability

please contact local marketing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
828 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durmuş

production target is April 29, for earlier availability

please contact local marketing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复