Hello,
I have implemented an OV5647 camera board which connects to my i.MX6 quad Wandboard. I am having trouble getting images from the driver and need some help figuring out why. I have reviewed about a dozen related threads on this forum, and tried to carefully implement their suggestions.
Here are the steps I have taken so far:
I have to guess that what is going on is that the image format is not being handled correctly, but I can't tell from the tracing.
Some specific questions:
The following is what I get with DEBUG tracing on in the drivers:
[ 1160.505314] End of mxc_v4l2_g_fmt: crop_current widthxheight 1280 x 960
[ 1160.505352] In MVC:mxc_v4l_ioctl
[ 1160.505360] In MVC: mxc_v4l_do_ioctl c0405602
[ 1160.505373] In MVC:mxc_v4l_ioctl
[ 1160.505380] In MVC: mxc_v4l_do_ioctl c0405602
[ 1160.505458] In MVC:mxc_v4l_ioctl
[ 1160.505465] In MVC: mxc_v4l_do_ioctl c0445624
[ 1160.505472] case default or not supported
[ 1160.505528] In MVC:mxc_v4l_ioctl
[ 1160.505535] In MVC: mxc_v4l_do_ioctl c02c563a
[ 1160.505540] case VIDIOC_CROPCAP
[ 1160.505547] In MVC:mxc_v4l_ioctl
[ 1160.505552] In MVC: mxc_v4l_do_ioctl 4014563c
[ 1160.505561] case VIDIOC_S_CROP
[ 1160.505567] Cropping Input to ipu size 1280 x 960
[ 1160.505678] In MVC:mxc_v4l_ioctl
[ 1160.505686] In MVC: mxc_v4l_do_ioctl c0145608
[ 1160.505693] case VIDIOC_REQBUFS
[ 1160.505697] In MVC:mxc_streamoff
[ 1160.505702] MVC: In mxc_free_frame_buf
[ 1160.505709] In MVC:mxc_allocate_frame_buf - size=152064
[ 1160.508739] In MVC:mxc_v4l_ioctl
[ 1160.508746] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.508752] case VIDIOC_QUERYBUF
[ 1160.508759] In MVC:mxc_v4l2_buffer_status
[ 1160.508904] In MVC:mxc_mmap
[ 1160.508911] pgoff=0x184c0, start=0x45dbd000, end=0x45de3000
[ 1160.508933] In MVC:mxc_v4l_ioctl
[ 1160.508939] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.508944] case VIDIOC_QUERYBUF
[ 1160.508949] In MVC:mxc_v4l2_buffer_status
[ 1160.508966] In MVC:mxc_mmap
[ 1160.508972] pgoff=0x18300, start=0x46549000, end=0x4656f000
[ 1160.508987] In MVC:mxc_v4l_ioctl
[ 1160.508992] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.508997] case VIDIOC_QUERYBUF
[ 1160.509002] In MVC:mxc_v4l2_buffer_status
[ 1160.509013] In MVC:mxc_mmap
[ 1160.509019] pgoff=0x18340, start=0x46700000, end=0x46726000
[ 1160.509033] In MVC:mxc_v4l_ioctl
[ 1160.509039] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.509044] case VIDIOC_QUERYBUF
[ 1160.509049] In MVC:mxc_v4l2_buffer_status
[ 1160.509058] In MVC:mxc_mmap
[ 1160.509064] pgoff=0x19f00, start=0x467ed000, end=0x46813000
[ 1160.509085] In MVC:mxc_v4l_ioctl
[ 1160.509092] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509097] case VIDIOC_QBUF
[ 1160.509104] In MVC:mxc_v4l_ioctl
[ 1160.509110] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509115] case VIDIOC_QBUF
[ 1160.509121] In MVC:mxc_v4l_ioctl
[ 1160.509126] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509131] case VIDIOC_QBUF
[ 1160.509138] In MVC:mxc_v4l_ioctl
[ 1160.509143] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509148] case VIDIOC_QBUF
[ 1160.509154] In MVC:mxc_v4l_ioctl
[ 1160.509160] In MVC: mxc_v4l_do_ioctl 40045612
[ 1160.509166] case VIDIOC_STREAMON
[ 1160.509170] In MVC:mxc_streamon
[ 1160.509175] IPU:In prp_enc_enabling_tasks
[ 1160.509981] In prp_enc_setup
[ 1160.509988] YUV420
[ 1160.510026] eba 184c0000
[ 1160.510033] eba 18300000
[ 1160.510230] In MVC:mxc_poll
[ 1160.510243] In MVC:mxc_v4l_ioctl
[ 1160.510250] In MVC: mxc_v4l_do_ioctl c0445611
[ 1160.510256] case VIDIOC_DQBUF
[ 1160.510261] In MVC:mxc_v4l_dqueue
[ 1170.504999] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
[ 1170.511966] In MVC:mxc_poll
[ 1170.511983] In MVC:mxc_v4l_ioctl
[ 1170.511991] In MVC: mxc_v4l_do_ioctl c0445611
[ 1170.511997] case VIDIOC_DQBUF
[ 1170.512001] In MVC:mxc_v4l_dqueue
[ 1180.504959] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
[ 1180.511757] In MVC:mxc_poll
[ 1180.511773] In MVC:mxc_v4l_ioctl
[ 1180.511783] In MVC: mxc_v4l_do_ioctl c0445611
[ 1180.511789] case VIDIOC_DQBUF
[ 1180.511794] In MVC:mxc_v4l_dqueue
[ 1190.504954] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
已解决! 转到解答。
[Edit Oct 24 2014: After receiving various messages from other users about what patches we have used, I have attached the relevant patches in a zip file. These contain the MT9M031 driver, OV5647 driver and changes to the freescale kernel to (1) enable Greyscale/Raw capture and (2) allow correctly synch'd capture from a MIPI channel other than channel 0]
I finally got it working a couple of days ago. I had a couple of problems but basically I hit and resolved the following issues:
At this point I am getting Bayer patter data in memory and will soon look into using the graphics coprocessor or IPU to handle demosaicing. When the code is a little cleaner I will also post my kernel patch and driver file.
Dave,
I am trying to make ov8865 sensor to work with wandboard dual by modifying the ov5640_mipi driver. All the I2C communication seems to be OK, then I get the same "ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0" error. Can you please clarify for me couple of thing from this post?
1) How can you see that "Driver reports data being received from sensor" ?
2) What's the "MIPI status register" ?
3) What' the setting to tell sensor to start streaming the MIPI data? Is it the 0x4202 register?
Thank you,
Lev.
Hi Lev,
I believe this means that we got 0x300 or 0x330 from the MIPI status register (I am going from memory here and it has been a long time). These values mean the MIPI bus is set up correctly and packets are being received on it. The MIPI status register is a register (documented in the i.MX6Q reference manual in the chapter on the MIPI to CSI gasket) which tells you whether the MIPI bus is able to communicate with your sensor or not.
Basically you have to tell your sensor to start sending frames using the I2C commands, and then you should start receiving data on the MIPI bus. Once you are receiving data correctly you have to make sure the data format and size are correct and that the correct capture channel is configured (for me this was CSI->MEM, not CSI->IPU->MEM (again going from memory, but something like that-- it had to be direct to memory since I wasn't decoding YUV).
The register to start streaming depends on your sensor. Contact your OmniVision rep for support. I didn't have any direct sales contact with OmniVision, and they still sent me the datasheets and provided register settings to get the OV5647 up and running.
If you're feeling lost, I was too. It took me a while to get my head around the data path, but once I did there were only two or three things to sort out. There is a somewhat helpful checklist on this forum:
https://community.freescale.com/docs/DOC-94312
Hope that helps,
Dave
Hi Dave McMordie / levlvovsky
Is there any driver for ov8865, which you know of ? We are planning to use ov8865 module with i.MX6Q processor.
Hi Vijai,
I have no idea if this device is supported as we do not use it. I would
suggest you post generally in a new topic to ask the question if you have
not already done so. If support is not offered, you will need register
settings from Omnivision’s support department and another driver for a
related sensor as a starting point. From there it is a messy road of
reading the datasheet and register reference, tweaking the driver, testing
and debugging.
Best,
Dave
From: Vijai Kumar
Sent: Tuesday, August 4, 2015 1:10 AM
To: Dave McMordie <mcmordie@viionsystems.com>
Subject: You have been mentioned by Vijai Kumar in Re: i.MX6 OV5647 Bayer
sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0)
in Freescale Community
<http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1pa/1sgFa3hhRMSf8pZgEF3etQ/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>
You have been mentioned
by Vijai Kumar
<http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1pa/1sgFa3hhRMSf8pZgEF3etQ/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRN-2FArDB1Dbz5vXUH-2BStRQn-2BONs1jeq5q4DHqLr40tzcMsi9vTZvKL7uhw2OMi-2Bqng-3D>
*in
Re: i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue
timeout enc_counter 0) in Freescale Community* - View Vijai Kumar's
reference to you
<http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1pa/1sgFa3hhRMSf8pZgEF3etQ/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTFPK2mrQBb99hPyShlgUemYgMLvNbG1ra5FN11uHtPyRB-2B30puStpr9Ysa0beN7B8-3D>
I got the sensor to send image data. For some reason I get data only when I set the sensor output to 8bit and declare image format as V4L2_PIX_FMT_GREY. If I declare format as V4L2_PIX_FMT_SBGGR8 bayer (which is right for that sensor in 8bit setting) then I get nothing. The data is also corrupted - rather than getting one big image I get 16 small images instead.
What the difference between CSI->MEM and CSI->IPU->MEM? I tried changing CSI->IPU->MEM to CSI->MEM but didn't notice any change. I think the Ov8865 sensor gives output only in the raw bayer format.
Thank you,
Lev.
[Edit Oct 24 2014: After receiving various messages from other users about what patches we have used, I have attached the relevant patches in a zip file. These contain the MT9M031 driver, OV5647 driver and changes to the freescale kernel to (1) enable Greyscale/Raw capture and (2) allow correctly synch'd capture from a MIPI channel other than channel 0]
I finally got it working a couple of days ago. I had a couple of problems but basically I hit and resolved the following issues:
At this point I am getting Bayer patter data in memory and will soon look into using the graphics coprocessor or IPU to handle demosaicing. When the code is a little cleaner I will also post my kernel patch and driver file.
Hi Dave,
Thanks for sharing the details of your work. I am working on to get a camera sensor working on a Wandboard Dual. The sensor appears to be somewhat similar to OV5647, at least in that sense that it is sending out the data over MIPI CSI-2 in raw Bayer 8 or 10bit format. I have now confirmed that I have the MIPI_CSI working properly as the DPHY status register is alternating between 0x300 and 0x330 during capture and the error bits are all clear. However, other than that, I get no data through the IPU pipeline. Looking at your description the reason for that is clear.
Therefore, I would be very much interested in seeing your code changes you have done. Have published them anywhere yet? Even if they are not cleaned up yet, I think those would be quite useful. Maybe I could somehow participate with fixing things as I appear to be facing the same problem here too.
Thanks!
Timo, did you check that virtual channel is properly set on the ov5647 side? I had the same outcome as you did working with ov9740 and the reason was that imx6 software expects vc=1 while ov9740 default is vc=0.
The virtual channel should be fine as I am getting the data all the way through to the gstreamer buffers and I am able save the captured image on a file.
Now the problem is that apparently the data that gets through is in the raw bayer format but the pixelformat information doesn't come correctly with the image stream. The data gets through if I configure the pixel format to V4L2_PIX_FMT_GREY, but that's not what the image data is really. If I configure the sensor and CSI2 into RAW10 mode, the captured image it looks like there are in fact four frames instead of one. That would make sense if the data that gets through is in bayer format but it is being interpreted as YUV or RGB. One reason for that is obviously the V4L2_PIX_FMT_GREY which I am using. Probably I need to add support for V4L2_PIX_FMT_SRGGB8 and V4L2_PIX_FMT_SRGGB10 at least.
But I haven't quite figured out yet how the data flows through the layers, so I am not there yet. I will let you know when I have some progress.
It sounds like you are well on the way if you are receiving the full
resolution bayer format images. I was not able to get the RG8/RG10
versions working—like you it returned an image which it had tried to colour
convert, and the result was a 4x4 grid of subimages. Since there I will
need to debayer the images in software anyhow, I left it at that. The
tracing I did do confirmed the correct CPMEM settings for each raw mode.
There are other threads in which some people report being able to capture
in RAW, but it was not clear to me how they got it working.
From: Timo Kokkonen
Sent: October-04-13 5:45 AM
To: Dave McMordie
Subject: Re: - i.MX6 OV5647 Bayer sensor driver (ERROR:
v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0)
<https://community.freescale.com/>
i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue
timeout enc_counter 0)
reply from Timo
Kokkonen<https://community.freescale.com/people/timokokkonen?et=watches.email.thread>in
i.MX Community - View the full
discussion<https://community.freescale.com/message/354072?et=watches.email.thread#354072>
Hi,
thanks for your reply.
Here's how it looks like
https://www.dropbox.com/s/8c2ww10qmk2s7h6/20150129_102941.jpg?dl=0
The images are stable, not scrolling, but you can see some slight color issues (seems to be a bit greenish) and the fact that it actually displays the frames in the space of a grid of 2 x 2. Sometimes it displays the entire 4 frames, sometimes like in the picture it displays some of the frames full and the others with some hsync and vsync issues.
So that is using V4L2_PIX_FMT_UYVY in my driver.
If I use V4L2_PIX_FMT_YUV420, I get a 2x4 grid
Subsequently, my driver enabled mipi using datatype:
mipi_csi2_set_datatype(mipi_csi2_info, MIPI_DT_YUV422);
Dump of registers:
IPUx_CSI0_SENS_CONF is 0x00008A32
IPUx_CSI0_ACT_FRM_SIZE is 0x023F02CF
Apparently IPUx_CSI0_SENS_CONF value shows data width is 8 bits. As I am receiving YUV422, shouldn't it read 16 bits instead?
It's 16 bits: 8 bits Y, 8 bits U, 8 bits Y, 8 bits V ---> 2 pixels (one Y for each of the 2 pixels, while U and V are shared between the 2 pixels)
So question remains: IPUx_CSI0_SENS_CONF should reflect through bits 14-11 the data format of the received data or is it something internal to CSI?
CSI0_DATA_WIDTH has the description - "Data width. This field defines the number of bits per color."
Not clear if it's the width of the received data or the width it will be sent internally to IPU.
Found this in the RM of imx6:
37.4.3.2.2
High-speed serial interface - MIPI (Mobile Industry Processor
Interface).
In MIPI interface two values arrive in each cycle. Each value is 8 bit wide, which means
16 MSB bits of the data bus input are treated, while 4 LSB bits are ignored.
When working in this mode, the CSI can handle up to 4 streams of data. Each stream is
identified with DI (data identifier) that includes the virtual channel and the data type of
this stream. Each stream that is handled is defined in registers MIPI_DI0-3. Only the
main stream (MIPI_DI0) can be sent to all destination units while the other streams are
sent only to the SMFC as generic data.
In this mode SENS_DATA_FORMAT and DATA_WIDTH registers are ignored, since
this information is coming to the CSI via the MCT_DI bus.
The only Bayer-related FOURCCs which the IPU Capture Driver would recognize are
#define IPU_PIX_FMT_GENERIC fourcc('I', 'P', 'U', '0') /*!< IPU Generic Data */
#define IPU_PIX_FMT_GENERIC_32 fourcc('I', 'P', 'U', '1') /*!< IPU Generic Data */
#define IPU_PIX_FMT_GENERIC_16 fourcc('I', 'P', 'U', '2') /*!< IPU Generic Data */
Formats "V4L2_PIX_FMT_SBGGR10" or "V4L2_PIX_FMT_SBGGR16" are not going to work.
Try 0x32555049 instead in your driver -- it is "IPU2" and will get data stream going.
Hi Timo,
My changes to the kernel can be found here:
I don’t have my camera driver up in a public place yet, but anyway that
won’t help you.
Basically there were substantial changes to enable grayscale mode and a
more minor change to get the MIPI clock rate right. It was also important
to use the correct image capture path (CSI->MEM) and to request the GRAY
format when capturing. Otherwise the drivers try to handle the colourspace
conversion and fail.
HTH,
D
From: Timo Kokkonen
Sent: October-02-13 9:26 AM
To: Dave McMordie
Subject: Re: - i.MX6 OV5647 Bayer sensor driver (ERROR:
v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0)
<https://community.freescale.com/>
i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue
timeout enc_counter 0)
reply from Timo
Kokkonen<https://community.freescale.com/people/timokokkonen?et=watches.email.thread>in
i.MX Community - View the full
discussion<https://community.freescale.com/message/353698?et=watches.email.thread#353698>