Dear sir/Madam,
We are using i.MX6Q custom board based on sabreSD board and we are using Linux-3.10.17_1.0.0-GA BSP for our development.
We have upgraded the RAM size into 2GB (earlier it was 1GB).
We would like to know the changes required in u-boot and Kernel for 2GB with below BSPs.
1. Linux-3.10.17_1.0.0-GA
2. L3.0.35_4.1.0_130816
Regards,
Ansari
Hello,
Please refer to Chapter 1 (Porting U-Boot from an i.MX 6 Reference
Board to an i.MX 6 Custom Board) of “i.MX_BSP_Porting_Guide.pdf” in
FSL Linux documentation.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------