i.MX6: Edge of the PWM output and the timing of VAL during complementary PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6: Edge of the PWM output and the timing of VAL during complementary PWM

812 Views
kenji
Contributor IV

Hi All

I would like to know the edge of the PWM output and the timing of VAL during complementary PWM.
There is little information in the document, and I would like to know the timing in the PWM mode I use.

kenji_0-1626692453166.png

 

[My PWM Setting]

kenji_1-1626692056330.png

kenji_2-1626692085830.png

 

 

Tags (1)
0 Kudos
Reply
3 Replies

781 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I'm not sure that I understood correctly, so please correct me if I'm wrong. Are you trying to know the value of the VALx registers, right? If so, these values are set inside the function PWM_SetupPwm. You can debug your application and see how these registers are being configured. 

Regards,
Victor 

 

0 Kudos
Reply

804 Views
jamesbone
NXP TechSupport
NXP TechSupport

 I apologize but your thread it is confusing, you  are mentioning i.Mx6 in the Subject, but you are adding Tags for the i.MXRT which device are you using?

 

 

0 Kudos
Reply

797 Views
kenji
Contributor IV

Hi jamesbone-san

 

I'm using MIMXRT1060-EVK(i.MX1062).

0 Kudos
Reply