Hello,
I am using i.MX53 QSB with Linux. I am facing problem with on board USB.
It is unable to populate the device USB devices. I have connected a
Dell Optical mouse(Model: MS111), on the serial console i could see the following prints.
and for about 20 iterations board gets restarted. I am using prebuilt linux images downloaded from freescale.com
usb 2-1: new low speed USB device using fsl-ehci and address 2
input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input4
generic-usb 0003:0461:4E22.0001: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0
usb 2-1: USB disconnect, address 2
usb 2-1: new low speed USB device using fsl-ehci and address 3
input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input5
generic-usb 0003:0461:4E22.0002: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0
usb 2-1: USB disconnect, address 3
usb 2-1: new low speed USB device using fsl-ehci and address 4
input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input6
generic-usb 0003:0461:4E22.0003: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0
usb 2-1: USB disconnect, address 4
usb 2-1: new low speed USB device using fsl-ehci and address 5
input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input7
generic-usb 0003:0461:4E22.0004: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0
usb 2-1: USB disconnect, address 5
after connecting the device "lsusb" output is
(no device detected)
Bus 001 Device 001: ID 1d6b:0002
Bus 002 Device 001: ID 1d6b:0002
Thanks and Regards
Priyatham.
please download the BSP (L2.6.35_11_09_ER_SOURCE) and apply the patches (IMX53_LINUX_1109_BSP_PATCH).
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
please try to build the image and then run it on the board.