i.MX 8QuadXPlus - MEK Default configuration and files "out-of-the-box"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8QuadXPlus - MEK Default configuration and files "out-of-the-box"

3,396 Views
viniciuscarvalho
Contributor II

Hello,

I would like some help to find/have the files and the setup procedure to return my development board as it was "out-of-the-box":
i.MX 8QuadXPlus Multisensory Enablement Kit | NXP Semiconductors

I couldn't find the files and the procedure to do it.

I have a HW B0 revision/version.

I'm trying to make it run with a LVDS-TO-HDMI bridge but I get no video output (nothing, no console, no blink, no noise, nothing). I would like to test if the LVDS-TO-HDMI bridge is burned or if I'm missing some configuration.

I already sent succefully the NXP image for Embedded Linux, Android and Android Automotive OS that are compatible with B0 revision.

The LVDS-TO-HDMI bridge is keeping the RED LED always ON and the GREEN LED after the kernel starts up.

From the COMM port I can see the "lvds-to-hdmi-bridge@4c" is being recognized by U-Boot.

On Embedded Linux, running on SD CARD, the kernel is initializing until it requests the login/password (root by default with blank password).

I can navigate into the folders "/dev", etc ... no problem.

Can anyone help me with that?

Thank you very much!






0 Kudos
Reply
8 Replies

2,985 Views
mano_zumi
Contributor I

facing the same issue with imx8qxp c0 mek. android boots fine facing display not coming up only with android automotive

0 Kudos
Reply

2,974 Views
viniciuscarvalho
Contributor II

In my case I can't see any video output, not even noises on the screen.

0 Kudos
Reply

3,351 Views
viniciuscarvalho
Contributor II

Hello, thanks for replying.

Android Automotive OS:
automotive-12.0.0_2.1.0_image_8qmek_car2

If I perform the boot procedure without setting:

setenv bootargs console=ttyLP0,115200 earlycon init=/init androidboot.fbTileSupport=enable cma=928M@0x960M-0xfc0M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware loop.max_part=7 transparent_hugepage=never moal.mod_para=wifi_mod_para.conf androidboot.lcd_density=240 bootconfig

The kernel starts and the LVDS-TO-HDMI bridge is turning the led green (but nothing is being display on the HDMI monitor connected to the bridge). After the kernel finishes the initialization I can navigate through the files/folders on the COMM (serial port)... but without video.

If I setenv as ANDROID_QUICK_START_GUIDE I don't have video, the LVDS-TO-HDMI bridge green led doesn't turn ON and the board keeps restarting during the kernel start-up (please see attached log).

I don't know what to do.

I would like to have the default files and configuration as "out-of-the-box" to check if my HW is OK.

Like this video:
Get Started with the MCIMX8QXP-CPU | NXP Semiconductors

Thank you!

0 Kudos
Reply

3,358 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Can you share which BSP you are facing this issue?

For Android OS, please refer 9.4.1 Booting with single LVDS-to-HDMI/MIPI-DSI-to-HDMI or dual LVDS-to-HDMI displays in  https://www.nxp.com/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf

Tags (1)

3,328 Views
viniciuscarvalho
Contributor II

Hello, thanks for replying.

Android Automotive OS:
automotive-12.0.0_2.1.0_image_8qmek_car2

If I perform the boot procedure without setting:

setenv bootargs console=ttyLP0,115200 earlycon init=/init androidboot.fbTileSupport=enable cma=928M@0x960M-0xfc0M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware loop.max_part=7 transparent_hugepage=never moal.mod_para=wifi_mod_para.conf androidboot.lcd_density=240 bootconfig

The kernel starts and the LVDS-TO-HDMI bridge is turning the led green (but nothing is being display on the HDMI monitor connected to the bridge). After the kernel finishes the initialization I can navigate through the files/folders on the COMM (serial port)... but without video.

If I setenv as ANDROID_QUICK_START_GUIDE I don't have video, the LVDS-TO-HDMI bridge green led doesn't turn ON and the board keeps restarting during the kernel start-up (please see attached log).

I don't know what to do.

I would like to have the default files and configuration as "out-of-the-box" to check if my HW is OK.

Like this video:
Get Started with the MCIMX8QXP-CPU | NXP Semiconductors

Thank you!

0 Kudos
Reply

3,349 Views
viniciuscarvalho
Contributor II

This is what I get when I try to boot using Linux (L5.4.24-2.1.0_images_MX8QXPMEK):

U-Boot 2020.04-5.4.24-2.1.0+g4979a99482 (May 30 2020 - 16:14:50 +0000)

CPU: NXP i.MX8QXP RevB A35 at 1200 MHz at 25C

Model: NXP i.MX8QXP MEK
Board: iMX8QXP MEK

BuildInfo:
- SCFW 4a1654e0, SECO-FW 376e3c15, IMX-MKIMAGE 6745ccdc, ATF b0a00f2
- U-Boot 2020.04-5.4.24-2.1.0+g4979a99482

Boot: MMC0
DRAM: 3 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0i2c: Error check busy bus: 0x8
it6263_i2c_reg_read, read err -102
faill to read from it6263 revision, ret -102
(1280 x 720)
[0] dpu@56180000, video
[1] lvds-channel@0, display
[2] lvds-to-hdmi-bridge@4c, video_bridge
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0(part 0) is current device
flash target is MMC:0
Net:
Warning: ethernet@5b040000 using MAC address from ROM
eth0: ethernet@5b040000 [PRIME]
Warning: ethernet@5b050000 (eth1) using random MAC address - da:dd:53:ac:0a:62
, eth1: ethernet@5b050000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
28021248 bytes read in 125 ms (213.8 MiB/s)
Booting from mmc ...
97270 bytes read in 9 ms (10.3 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 0000000083000000, end 000000008301abf5
Disable clock-controller@5a4d0000 rsrc 62 not owned
Disable clock-controller@5ac90000 rsrc 102 not owned

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd042]
[ 0.000000] Linux version 5.4.24-2.1.0+gbabac008e5cf (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Sat May 30 14:53:48 UTC 2020
[ 0.000000] Machine model: Freescale i.MX8QXP MEK
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090000000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0vring0@90000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090008000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0vring1@90008000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090010000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev1vring0@90010000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090018000, size 0 MiB
[ 0.000000] OF: reserved mem: initialized node vdev1vring1@90018000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[ 0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x00000008bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x8bf9f8500-0x8bf9f9fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000080200000-0x00000000ffffffff]
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008bfffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000086200000-0x0000000087ffffff]
[ 0.000000] node 0: [mem 0x0000000090020000-0x00000000901fffff]
[ 0.000000] node 0: [mem 0x0000000090500000-0x0000000091ffffff]
[ 0.000000] node 0: [mem 0x0000000094c00000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000008bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 720940
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0xfbfff000-0xfffff000] (64MB)
[ 0.000000] Memory: 1790216K/2929536K available (16444K kernel code, 1444K rwdata, 6472K rodata, 2944K init, 1017K bss, 156280K reserved, 983040K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 512 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008872] Console: colour dummy device 80x25
[ 0.013060] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.023230] pid_max: default: 32768 minimum: 301
[ 0.027918] LSM: Security Framework initializing
[ 0.032505] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.039834] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.071738] ASID allocator initialised with 32768 entries
[ 0.084833] rcu: Hierarchical SRCU implementation.
[ 0.099670] EFI services will not be available.
[ 0.111906] smp: Bringing up secondary CPUs ...
[ 0.148534] Detected VIPT I-cache on CPU1
[ 0.148565] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[ 0.148605] CPU1: Booted secondary processor 0x0000000001 [0x410fd042]
[ 0.180577] Detected VIPT I-cache on CPU2
[ 0.180599] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000
[ 0.180623] CPU2: Booted secondary processor 0x0000000002 [0x410fd042]
[ 0.212640] Detected VIPT I-cache on CPU3
[ 0.212660] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000
[ 0.212682] CPU3: Booted secondary processor 0x0000000003 [0x410fd042]
[ 0.212753] smp: Brought up 1 node, 4 CPUs
[ 0.268647] SMP: Total of 4 processors activated.
[ 0.273335] CPU features: detected: 32-bit EL0 Support
[ 0.278474] CPU features: detected: CRC32 instructions
[ 0.290675] CPU: All CPU(s) started at EL2
[ 0.294472] alternatives: patching kernel code
[ 0.300146] devtmpfs: initialized
[ 0.319080] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.328506] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.367350] pinctrl core: initialized pinctrl subsystem
[ 0.373390] DMI not present or invalid.
[ 0.377222] NET: Registered protocol family 16
[ 0.389977] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.395772] audit: initializing netlink subsys (disabled)
[ 0.401409] audit: type=2000 audit(0.344:1): state=initialized audit_enabled=0 res=1
[ 0.408886] cpuidle: using governor menu
[ 0.413831] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.422292] Serial: AMBA PL011 UART driver
[ 0.426131] imx mu driver is registered.
[ 0.429972] imx rpmsg driver is registered.
[ 0.496753] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.503138] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.509814] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.516505] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.525270] cryptd: max_cpu_qlen set to 1000
[ 0.537123] ACPI: Interpreter disabled.
[ 0.543164] iommu: Default domain type: Translated
[ 0.547922] vgaarb: loaded
[ 0.550772] SCSI subsystem initialized
[ 0.554688] usbcore: registered new interface driver usbfs
[ 0.559885] usbcore: registered new interface driver hub
[ 0.565199] usbcore: registered new device driver usb
[ 0.572898] mc: Linux media interface: v0.10
[ 0.576885] videodev: Linux video capture interface: v2.00
[ 0.582395] pps_core: LinuxPPS API ver. 1 registered
[ 0.587257] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.596389] PTP clock support registered
[ 0.600743] EDAC MC: Ver: 3.0.0
[ 0.605347] No BMan portals available!
[ 0.609150] QMan: Allocated lookup table at (____ptrval____), entry count 65537
[ 0.616839] No QMan portals available!
[ 0.621296] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 0.628185] FPGA manager framework
[ 0.631355] Advanced Linux Sound Architecture Driver Initialized.
[ 0.637828] Bluetooth: Core ver 2.22
[ 0.641084] NET: Registered protocol family 31
[ 0.645497] Bluetooth: HCI device and connection manager initialized
[ 0.651843] Bluetooth: HCI socket layer initialized
[ 0.656705] Bluetooth: L2CAP socket layer initialized
[ 0.661752] Bluetooth: SCO socket layer initialized
[ 0.667999] imx-scu scu: NXP i.MX SCU Initialized
[ 0.678174] random: fast init done
[ 0.719262] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[ 0.728777] imx8qxp-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[ 0.737610] clocksource: Switched to clocksource arch_sys_counter
[ 0.743591] VFS: Disk quotas dquot_6.6.0
[ 0.747718] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.755268] pnp: PnP ACPI: disabled
[ 0.789569] thermal_sys: Registered thermal governor 'step_wise'
[ 0.789575] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.795834] NET: Registered protocol family 2
[ 0.806800] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.815053] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.823130] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.830716] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.837043] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.843679] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.850934] NET: Registered protocol family 1
[ 0.855525] RPC: Registered named UNIX socket transport module.
[ 0.861123] RPC: Registered udp transport module.
[ 0.865802] RPC: Registered tcp transport module.
[ 0.870495] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.877402] PCI: CLS 0 bytes, default 64
[ 0.881870] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.890601] kvm [1]: IPA Size Limit: 40bits
[ 0.895219] kvm [1]: GICv3: no GICV resource entry
[ 0.899681] kvm [1]: disabling GICv2 emulation
[ 0.904126] kvm [1]: GIC system register CPU interface enabled
[ 0.910005] kvm [1]: vgic interrupt IRQ1
[ 0.913966] kvm [1]: Hyp mode initialized successfully
[ 0.926125] Initialise system trusted keyrings
[ 0.930390] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[ 0.944394] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.950728] NFS: Registering the id_resolver key type
[ 0.955483] Key type id_resolver registered
[ 0.959614] Key type id_legacy registered
[ 0.963616] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.970316] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.976857] 9p: Installing v9fs 9p2000 file system support
[ 0.999298] Key type asymmetric registered
[ 1.003064] Asymmetric key parser 'x509' registered
[ 1.007978] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 1.015310] io scheduler mq-deadline registered
[ 1.019824] io scheduler kyber registered
[ 1.046186] imx6q-pcie 5f010000.pcie: couldn't get pcie-phy
[ 1.050524] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 1.061291] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 1.072160] EINJ: ACPI disabled.
[ 1.161746] mxs-dma 5b810000.dma-apbh: initialized
[ 1.169968] Bus freq driver module loaded
[ 1.183629] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.195746] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 58, base_baud = 5000000) is a FSL_LPUAR[ 1.204922] printk: console [ttyLP0] enabled
[ 1.204922] printk: console [ttyLP0] enabled
[ 1.213343] printk: bootconsole [lpuart32] disabled
[ 1.213343] printk: bootconsole [lpuart32] disabled
[ 1.223483] fsl-lpuart 5a060000.serial: DMA tx channel request failed, operating without tx DMA
[ 1.232207] fsl-lpuart 5a060000.serial: DMA rx channel request failed, operating without rx DMA
[ 1.241455] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 59, base_baud = 5000000) is a FSL_LPUART
[ 1.251803] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 60, base_baud = 5000000) is a FSL_LPUART
[ 1.262129] 5a090000.serial: ttyLP3 at MMIO 0x5a090010 (irq = 61, base_baud = 5000000) is a FSL_LPUART
[ 1.340037] loop: module loaded
[ 1.349120] imx ahci driver is registered.
[ 1.364158] spi-nor spi0.0: mt35xu512aba (65536 Kbytes)
[ 1.377753] libphy: Fixed MDIO Bus: probed
[ 1.382873] tun: Universal TUN/TAP device driver, 1.6
[ 1.390820] thunder_xcv, ver 1.0
[ 1.394107] thunder_bgx, ver 1.0
[ 1.397372] nicpf, ver 1.0
[ 1.402370] pps pps0: new PPS source ptp0
[ 1.413037] libphy: fec_enet_mii_bus: probed
[ 1.418871] fec 5b040000.ethernet eth0: registered PHC device 0
[ 1.427186] Freescale FM module, FMD API version 21.1.0
[ 1.433462] Freescale FM Ports module
[ 1.437182] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 1.443474] fsl_dpa: FSL DPAA Ethernet driver
[ 1.448292] fsl_advanced: FSL DPAA Advanced drivers:
[ 1.453267] fsl_proxy: FSL DPAA Proxy initialization driver
[ 1.459276] fsl_oh: FSL FMan Offline Parsing port driver
[ 1.467583] hclge is initializing
[ 1.470921] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.478153] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.483552] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 1.490618] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.496410] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.502259] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.508248] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 1.515226] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.520848] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.528689] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.535181] sky2: driver version 1.30
[ 1.541882] VFIO - User Level meta-driver version: 0.3
[ 1.554342] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.560898] ehci-pci: EHCI PCI platform driver
[ 1.565427] ehci-platform: EHCI generic platform driver
[ 1.571434] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.577658] ohci-pci: OHCI PCI platform driver
[ 1.582178] ohci-platform: OHCI generic platform driver
[ 1.589778] usbcore: registered new interface driver usb-storage
[ 1.595898] usbcore: registered new interface driver usbserial_generic
[ 1.602463] usbserial: USB Serial support registered for generic
[ 1.608507] usbcore: registered new interface driver ftdi_sio
[ 1.614338] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.621725] usbcore: registered new interface driver usb_serial_simple
[ 1.628290] usbserial: USB Serial support registered for carelink
[ 1.634409] usbserial: USB Serial support registered for zio
[ 1.640100] usbserial: USB Serial support registered for funsoft
[ 1.646137] usbserial: USB Serial support registered for flashloader
[ 1.652525] usbserial: USB Serial support registered for google
[ 1.658475] usbserial: USB Serial support registered for libtransistor
[ 1.665034] usbserial: USB Serial support registered for vivopay
[ 1.671070] usbserial: USB Serial support registered for moto_modem
[ 1.677371] usbserial: USB Serial support registered for motorola_tetra
[ 1.684015] usbserial: USB Serial support registered for novatel_gps
[ 1.690399] usbserial: USB Serial support registered for hp4x
[ 1.696177] usbserial: USB Serial support registered for suunto
[ 1.702131] usbserial: USB Serial support registered for siemens_mpi
[ 1.720209] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 1.732194] imx-sc-rtc scu:rtc: registered as rtc0
[ 1.738335] i2c /dev entries driver
[ 1.751798] Bluetooth: HCI UART driver ver 2.3
[ 1.756286] Bluetooth: HCI UART protocol H4 registered
[ 1.761449] Bluetooth: HCI UART protocol BCSP registered
[ 1.766797] Bluetooth: HCI UART protocol LL registered
[ 1.771952] Bluetooth: HCI UART protocol ATH3K registered
[ 1.777382] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.784026] Bluetooth: HCI UART protocol Broadcom registered
[ 1.789732] Bluetooth: HCI UART protocol QCA registered
[ 1.802167] sdhci: Secure Digital Host Controller Interface driver
[ 1.808412] sdhci: Copyright(c) Pierre Ossman
[ 1.813512] Synopsys Designware Multimedia Card Interface Driver
[ 1.821872] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.829915] mmc0: CQHCI version 5.10
[ 1.865060] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 1.873271] mmc1: CQHCI version 5.10
[ 1.883133] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.892104] caam 31400000.crypto: device ID = 0x0a16040000000100 (Era 9)
[ 1.898859] caam 31400000.crypto: job rings = 2, qi = 0
[ 1.931611] caam algorithms registered in /proc/crypto
[ 1.940053] caam 31400000.crypto: caam pkc algorithms registered in /proc/crypto
[ 1.948347] caam_jr 31430000.jr: registering rng-caam
[ 1.960345] usbcore: registered new interface driver usbhid
[ 1.965977] usbhid: USB HID core driver
[ 1.970540] mxc-md bus@58000000:camera: deferring cap_device device registration
[ 1.981711] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[ 1.989159] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[ 1.996587] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[ 2.004015] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[ 2.011437] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[ 2.037641] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0
[ 2.044296] mmc0: new HS400 MMC card at address 0001
[ 2.046334] mxc-parallel-csi 58261000.pcsi: mxc_parallel_csi_probe probe successfully
[ 2.049961] mmcblk0: mmc0:0001 R1J57L 29.1 GiB
[ 2.059618] No fsl,qman node
[ 2.061973] mmcblk0boot0: mmc0:0001 R1J57L partition 1 8.00 MiB
[ 2.064562] Freescale USDPAA process driver
[ 2.070727] mmcblk0boot1: mmc0:0001 R1J57L partition 2 8.00 MiB
[ 2.074668] fsl-usdpaa: no region found
[ 2.074671] Freescale USDPAA process IRQ driver
[ 2.078387] imx-rproc imx8x_cm4@0: failed to find syscon
[ 2.080798] mmcblk0rpmb: mmc0:0001 R1J57L partition 3 4.00 MiB, chardev (237:0)
[ 2.084581] remoteproc remoteproc0: releasing imx-rproc
[ 2.107070] mmcblk0: p1 p2
[ 2.121685] Galcore version 6.4.0.234062
[ 2.328553] imx-cs42888 sound-cs42888: failed to find codec platform device
[ 2.336238] imx-wm8960 sound-wm8960: failed to find codec platform device
[ 2.345067] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59820000
[ 2.352207] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59830000
[ 2.359511] debugfs: Directory '59820000.sai' with parent 'imx-audmix' already present!
[ 2.367615] debugfs: Directory '59830000.sai' with parent 'imx-audmix' already present!
[ 2.375888] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> 59820000.sai mapping ok
[ 2.383604] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> 59830000.sai mapping ok
[ 2.391266] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> audmix-0 mapping ok
[ 2.398556] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> audmix-1 mapping ok
[ 2.405834] imx-audmix imx-audmix.0: ASoC: no DMI vendor name!
[ 2.417722] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 2.425861] NET: Registered protocol family 26
[ 2.431124] NET: Registered protocol family 10
[ 2.436421] Segment Routing with IPv6
[ 2.440178] NET: Registered protocol family 17
[ 2.444764] Bluetooth: RFCOMM TTY layer initialized
[ 2.449668] Bluetooth: RFCOMM socket layer initialized
[ 2.454920] Bluetooth: RFCOMM ver 1.11
[ 2.458696] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.464024] Bluetooth: BNEP filters: protocol multicast
[ 2.469266] Bluetooth: BNEP socket layer initialized
[ 2.474237] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.480190] Bluetooth: HIDP socket layer initialized
[ 2.485208] 8021q: 802.1Q VLAN Support v1.8
[ 2.489417] lib80211: common routines for IEEE802.11 drivers
[ 2.495236] 9pnet: Installing 9P2000 support
[ 2.499581] tsn generic netlink module v1 init...
[ 2.504397] Key type dns_resolver registered
[ 2.509195] registered taskstats version 1
[ 2.513312] Loading compiled-in X.509 certificates
[ 2.545141] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[ 2.572502] usb_phy_generic bus@5b000000:usb3-phy: bus@5b000000:usb3-phy supply vcc not found, using dummy regulator
[ 2.584056] gpio-42 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[ 2.592974] imx-lpi2c 37230000.i2c: using scl,sda for recovery
[ 2.606398] ov5640 16-003c: 16-003c supply DOVDD not found, using dummy regulator
[ 2.613986] ov5640 16-003c: 16-003c supply AVDD not found, using dummy regulator
[ 2.621447] ov5640 16-003c: 16-003c supply DVDD not found, using dummy regulator
[ 2.676333] ov5640 16-003c: ov5640_read_reg: error: reg=300a
[ 2.682037] ov5640 16-003c: ov5640_check_chip_id: failed to read chip identifier
[ 2.690503] ov5640: probe of 16-003c failed with error -5
[ 2.696007] i2c i2c-16: LPI2C adapter registered
[ 2.703029] max732x 18-0068: failed reading
[ 2.707275] max732x: probe of 18-0068 failed with error -5
[ 2.712923] i2c i2c-17: Added multiplexed i2c bus 18
[ 2.718142] i2c i2c-17: Added multiplexed i2c bus 19
[ 2.724431] input: fxos8700 as /devices/platform/bus@5a000000/5a810000.i2c/i2c-17/i2c-20/20-001e/input/input1
[ 2.736249] fxos8700 device driver probe successfully
[ 2.737061] input: fxas2100x as /devices/platform/bus@5a000000/5a810000.i2c/i2c-17/i2c-20/20-0021/input/input2
[ 2.752880] fxas2100x 20-0021: fxas2100x device driver probe successfully
[ 2.760300] read mpl3115 chip id 0xc4
[ 2.764114] input: mpl3115 as /devices/virtual/input/input3
[ 2.770405] mpl3115 device driver probe successfully
[ 2.770467] i2c i2c-17: Added multiplexed i2c bus 20
[ 2.783443] isl29023 21-0044: 21-0044 supply vdd not found, using dummy regulator
[ 2.797243] input: isl29023 light sensor as /devices/virtual/input/input4
[ 2.804457] isl29023 21-0044: driver version 1.0 enabled
[ 2.809874] i2c i2c-17: Added multiplexed i2c bus 21
[ 2.814866] pca954x 17-0071: registered 4 multiplexed busses for I2C switch pca9646
[ 2.823506] OF: graph: no port node found in /bus@5a000000/i2c@5a810000/tcpc@50
[ 2.831708] i2c i2c-17: LPI2C adapter registered
[ 2.849776] max9286_mipi 22-006a: max9286_read_reg:read reg error: reg=1e
[ 2.856619] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[ 2.862849] i2c i2c-22: LPI2C adapter registered
[ 2.868014] imx-lpi2c 56226000.i2c: can't get irq number
[ 2.875075] imx-lpi2c 56246000.i2c: can't get irq number
[ 2.884591] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 2.884720] imx6q-pcie 5f010000.pcie: couldn't get pcie-phy
[ 2.895743] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 2.901055] imx6q-pcie 5f010000.pcie: 5f010000.pcie supply epdev_on not found, using dummy regulator
[ 2.916663] dpu-core 56180000.dpu: driver probed
[ 2.918941] imx6q-pcie 5f010000.pcie: No cache used with register defaults set!
[ 2.925286] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.931993] imx6q-pcie 5f010000.pcie: host bridge /bus@5f000000/pcie@0x5f010000 ranges:
[ 2.937320] [drm] No driver support for vblank timestamp query.
[ 2.937404] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 2.945387] imx6q-pcie 5f010000.pcie: IO 0x7ff80000..0x7ff8ffff -> 0x00000000
[ 2.951663] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 2.959401] imx6q-pcie 5f010000.pcie: MEM 0x70000000..0x7fefffff -> 0x70000000
[ 2.967149] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 2.989036] imx-drm display-subsystem: failed to bind bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops): -517
[ 2.999041] imx-drm display-subsystem: master bind failed: -517
[ 3.013849] mmc1: CQHCI version 5.10
[ 3.017487] sdhci-esdhc-imx 5b020000.mmc: Got CD GPIO
[ 3.022589] sdhci-esdhc-imx 5b020000.mmc: Got WP GPIO
[ 3.059322] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA
[ 3.073188] mx8-img-md: Registered mxc_isi.0.capture as /dev/video0
[ 3.079815] mx8-img-md: Registered mxc_isi.1.capture as /dev/video1
[ 3.081644] imx6q-pcie 5f010000.pcie: PCIe PLL locked after 0 us.
[ 3.086383] mx8-img-md: Registered mxc_isi.2.capture as /dev/video2
[ 3.098768] mx8-img-md: Registered mxc_isi.3.capture as /dev/video3
[ 3.105346] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 3.112019] unregister ISI channel: mxc_isi.0
[ 3.116498] unregister ISI channel: mxc_isi.1
[ 3.120967] unregister ISI channel: mxc_isi.2
[ 3.125434] unregister ISI channel: mxc_isi.3
[ 3.129969] unregister ISI channel: mxc_isi.4
[ 3.135397] imx-rproc imx8x_cm4@0: failed to find syscon
[ 3.140901] imx-rproc imx8x_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb"
[ 3.150230] imx-rproc imx8x_cm4@0: No txdb, ret 0
[ 3.155569] remoteproc remoteproc0: imx-rproc is available
[ 3.162433] imx-cs42888 sound-cs42888: failed to find codec platform device
[ 3.171030] debugfs: Directory '59050000.sai' with parent 'wm8960-audio' already present!
[ 3.179365] imx-wm8960 sound-wm8960: wm8960-hifi <-> 59050000.sai mapping ok
[ 3.186482] imx-wm8960 sound-wm8960: ASoC: no DMI vendor name!
[ 3.306581] can-stby: supplied by can-en
[ 3.330531] cs42xx8 16-0048: failed to get device ID, ret = -5
[ 3.336673] cs42xx8: probe of 16-0048 failed with error -5
[ 3.343957] OF: graph: no port node found in /bus@5a000000/i2c@5a810000/tcpc@50
[ 4.085706] imx6q-pcie 5f010000.pcie: Phy link never came up
[ 4.091482] imx6q-pcie 5f010000.pcie: failed to initialize host
[ 4.097424] imx6q-pcie 5f010000.pcie: unable to add pcie port.
[ 4.421875] it6263 23-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[ 4.429639] adv7511 23-003d: 23-003d supply avdd not found, using dummy regulator
[ 4.437220] adv7511 23-003d: 23-003d supply dvdd not found, using dummy regulator
[ 4.444778] adv7511 23-003d: 23-003d supply pvdd not found, using dummy regulator
[ 4.452334] adv7511 23-003d: 23-003d supply a2vdd not found, using dummy regulator
[ 4.459969] adv7511 23-003d: 23-003d supply v3p3 not found, using dummy regulator
[ 4.467552] adv7511 23-003d: 23-003d supply v1p2 not found, using dummy regulator
[ 5.481659] adv7511 23-003d: Probe failed. Remote port 'dsi_host@56228000' disabled
[ 5.489418] i2c i2c-23: LPI2C adapter registered
[ 5.551051] it6263 24-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[ 5.558727] adv7511 24-003d: 24-003d supply avdd not found, using dummy regulator
[ 5.566303] adv7511 24-003d: 24-003d supply dvdd not found, using dummy regulator
[ 5.574390] adv7511 24-003d: 24-003d supply pvdd not found, using dummy regulator
[ 5.581935] adv7511 24-003d: 24-003d supply a2vdd not found, using dummy regulator
[ 5.589572] adv7511 24-003d: 24-003d supply v3p3 not found, using dummy regulator
[ 5.597123] adv7511 24-003d: 24-003d supply v1p2 not found, using dummy regulator
[ 5.605101] adv7511 24-003d: Probe failed. Remote port 'dsi_host@56248000' disabled
[ 5.612850] i2c i2c-24: LPI2C adapter registered
[ 5.618726] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 5.625362] [drm] No driver support for vblank timestamp query.
[ 5.631370] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 5.639653] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 5.647034] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 5.654690] imx-drm display-subsystem: bound bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops)
[ 5.663182] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
[ 5.671830] imx-drm display-subsystem: bound bus@56220000:ldb@562410e0 (ops imx8qxp_ldb_ops)
[ 5.680336] imx-drm display-subsystem: bound 56248000.dsi_host (ops nwl_dsi_component_ops)
[ 5.689052] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[ 5.706243] imx-cs42888 sound-cs42888: failed to find codec platform device
[ 5.715330] imx-cs42888 sound-cs42888: failed to find codec platform device
[ 5.725333] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[ 5.733074] debugfs: Directory 'mipi1-i2c1' with parent 'pm_genpd' already present!
[ 5.740759] debugfs: Directory 'mipi1-i2c0' with parent 'pm_genpd' already present!
[ 5.748451] debugfs: Directory 'mipi1-pwm0' with parent 'pm_genpd' already present!
[ 5.756127] debugfs: Directory 'mipi1' with parent 'pm_genpd' already present!
[ 5.771793] imx-sc-rtc scu:rtc: setting system clock to 2022-08-05T07:41:59 UTC (1659685319)
[ 5.782447] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[ 5.790803] imx-cs42888 sound-cs42888: failed to find codec platform device
[ 5.798014] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 5.807018] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 5.813673] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 5.822311] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 5.840383] ALSA device list:
[ 5.843373] #0: imx-audmix
[ 5.846273] #1: wm8960-audio
[ 5.856806] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 5.865055] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 5.871534] devtmpfs: mounted
[ 5.875498] Freeing unused kernel memory: 2944K
[ 5.880153] Run /sbin/init as init process
[ 5.988919] systemd[1]: systemd 243.2+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 6.011170] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)!

[ 6.066612] systemd[1]: Set hostname to <imx8qxpmek>.
[ 6.076339] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.083100] systemd[1]: Initializing machine ID from random generator.
[ 6.310989] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus/system_bus_socket → /run/dbus/system_bus_socket; please update the unit file accordingly.
[ 6.341216] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/syslogd.pid → /run/syslogd.pid; please update the unit file accordingly.
[ 6.375021] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/rpcbind.sock → /run/rpcbind.sock; please update the unit file accordingly.
[ 6.399483] systemd[1]: /lib/systemd/system/klogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/klogd.pid → /run/klogd.pid; please update the unit file accordingly.
[ 6.540814] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.547713] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 6.560124] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ OK ] Created slice system-getty.slice.
[ 6.581777] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice User and Session Slice.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target Paths.
[ OK ] Reached target Remote File Systems.
[ OK ] Reached target Slices.
[ OK ] Reached target Swap.
[ OK ] Listening on Syslog Socket.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on Journal Audit Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on udev Kernel Socket.
Mounting Huge Pages File System...
Mounting POSIX Message Queue File System...
Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...
Starting Create list of st…odes for the current kernel...
Starting Journal Service...
Mounting Kernel Configuration File System...
Starting Remount Root and Kernel File Systems...
Starting Apply Kernel Variables...
[ 6.954566] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting udev Coldplug all Devices...
Starting Setup Virtual Console...
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Started Journal Service.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta… nodes for the current kernel.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Setup Virtual Console.
Starting Flush Journal to Persistent Storage...
[ 7.170503] systemd-journald[460]: Received client request to flush runtime journal.
Starting Create System Users...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Run pending postinsts...
Starting Rebuild Journal Catalog...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Network Time Synchronization.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
Starting Start Psplash Boot Screen...
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Started Run pending postinsts.
[ 8.178399] [VPU Encoder] enable mu for core[0]
[ 8.191465] [VPU Encoder] vpu encoder core[0] firmware version is 1.2.7
[ 8.267610] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video1 (81,3)
[ 8.279693] imx-cs42888 sound-cs42888: failed to find codec platform device
[ OK ] Started Rebuild Dynamic Linker Cache.
Starting Update is Completed...
[ OK ] Started Update is Completed.
[ 8.337660] CAN device driver interface
[ 8.337936] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video2 (81,4)
[ OK ] Reached target System Initialization.
[ 8.351349] imx-cs42888 sound-cs42888: failed to find codec platform device
[ OK ] Started Daily apt download activities.
[ 8.372537] imx-cs42888 sound-cs42888: failed to find codec platform device
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ 8.403290] imx-cs42888 sound-cs42888: failed to find codec platform device
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
Starting Console System Startup Logging...
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
Starting Packet Filtering Framework...
Starting Network Time Service (one-shot ntpdate mode)...
Starting Telephony service...
[ OK ] Started Updates psplash to basic.
[ OK ] Started User Space Regulatory Firmware Loading.
Starting RPC Bind Service...
[ OK ] Started User Space SDMA Firmware Loading.
Starting System Logging Service...
Starting Login Service...
[ OK ] Started TEE Supplicant.
[ OK ] Started Console System Startup Logging.
[ OK ] Started Packet Filtering Framework.
[ OK ] Started Network Time Service (one-shot ntpdate mode).
[ OK ] Started RPC Bind Service.
[ OK ] Started System Logging Service.
[ OK ] Started Telephony service.
[ OK ] Started Login Service.
[ OK ] Created slice system-systemd\x2dbacklight.slice.
[ OK ] Created slice system-weston.slice.
[ OK ] Reached target Network (Pre).
Starting Save/Restore Sound Card State...
Starting Connection service...
Starting Kernel Logging Service...
Starting Load/Save Screen … backlight:lvds_backlight@0...
Starting Load/Save Screen … backlight:lvds_backlight@1...
Starting Network Service...
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Started Load/Save Screen B…of backlight:lvds_backlight@0.
[ OK ] Started Load/Save Screen B…of backlight:lvds_backlight@1.
[ OK ] Started Connection service.
[ OK [ 9.585955] Atheros 8031 ethernet 5b040000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
] Started Network Service.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Reached target Sound Card.
Starting Avahi mDNS/DNS-SD Stack...
Starting Hostname Service...
Starting WPA supplicant...
[ OK ] Found device /dev/mmcblk0p1.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started WPA supplicant.
[ OK ] Reached target Network.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Update psplash to network.
Starting Terminate Psplash Boot Screen...
Starting /etc/rc.local Compatibility...
Starting File System Check on /dev/mmcblk0p1...
Starting Permit User Sessions...
[ OK ] Started Kernel Logging Service.
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Started Permit User Sessions.
[ OK ] Started Hostname Service.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyLP0.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
Starting Weston Wayland Compositor (on tty7)...
[ OK ] Started Weston Wayland Compositor (on tty7).
[ OK ] Started File System Check on /dev/mmcblk0p1.
Mounting /run/media/mmcblk0p1...
[ OK ] Mounted /run/media/mmcblk0p1.
[ OK ] Started Update UTMP about System Runlevel Changes.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 10.312617] audit: type=1006 audit(1659685324.036:2): pid=751 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of user root.
[ 12.017655] random: crng init done
[ 12.021074] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.

NXP i.MX Release Distro 5.4-zeus imx8qxpmek ttyLP0

imx8qxpmek login: root
Last login: Fri Aug 5 07:42:03 UTC 2022 on tty7
root@imx8qxpmek:~#
root@imx8qxpmek:~#
root@imx8qxpmek:~#
root@imx8qxpmek:~#
root@imx8qxpmek:~#
root@imx8qxpmek:~#
root@imx8qxpmek:~# [ 35.893655] SD1_SPWR: disabling
[ 35.896813] can-en: disabling
[ 35.899825] can-stby: disabling
[ 35.903011] usb_otg1_vbus: disabling
^C
root@imx8qxpmek:~#

The LVDS-TO-HDMI bridge green LED turns ON but nothing is happening on the HDMI monitor.

0 Kudos
Reply

3,047 Views
NajiyaNazrin
Contributor I

Hi , I'm facing the same issue here. Im using IMX8QUADXPLUS  and HDMI output is not showing . Is the issue resolved for you? @viniciuscarvalho 

0 Kudos
Reply

2,975 Views
viniciuscarvalho
Contributor II

No, I bought a new LVDS-TO-HDMI converter to test it. But, I don't think that the problem is the HW.

0 Kudos
Reply