how to flash demo image to SD card for Android OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to flash demo image to SD card for Android OS

跳至解决方案
2,116 次查看
Ruban1
Contributor II

how to flash demo image to SD card for Android OS

I have downloaded 11.0.0_1.0.0_DEMO_8MM for imx8m mini evk board

I have gone through all the pdf recommended by NXP.

Can you provide me only the command required to flash demo image to SD card.

And should i place SD card in card reader and connect to Ubuntu PC and RUN the command and after flashing done .Then insert SD card to imx8m mini evk board then switch to SD card mode and ON the board.

Or should insert SD card inside imx8m mini evk board then which mode should i select.

If download mode how to connect with PC through C type or B type and using minicom .

After flashing through download mode . should i change to SD card mode and ON the board.

There are 2 method of flashing . Can you provide command and procedure for each method

such as  UUU with command and procedure and other using Fastboot with command and procedure.

0 项奖励
回复
1 解答
2,114 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

And should i place SD card in card reader and connect to Ubuntu PC and RUN the command and after flashing done .Then insert SD card to imx8m mini evk board then switch to SD card mode and ON the board.

>>>No, just put sd in board, and switch download mode, using uuu

sudo ./uuu_imx_android_flash.bat -f imx8mm -t sd -a -e -u dual -d mipi-panel

 

After flashing through download mode . should i change to SD card mode and ON the board.

>>>>Yes

 

We recommad you uuu, it will save you a lot of time.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,115 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

And should i place SD card in card reader and connect to Ubuntu PC and RUN the command and after flashing done .Then insert SD card to imx8m mini evk board then switch to SD card mode and ON the board.

>>>No, just put sd in board, and switch download mode, using uuu

sudo ./uuu_imx_android_flash.bat -f imx8mm -t sd -a -e -u dual -d mipi-panel

 

After flashing through download mode . should i change to SD card mode and ON the board.

>>>>Yes

 

We recommad you uuu, it will save you a lot of time.

0 项奖励
回复
2,107 次查看
Ruban1
Contributor II

and through which port should connect ..using c type or USB type B that mini USB

 

0 项奖励
回复
2,092 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Download:TypeC

Uart debug: micro usb

0 项奖励
回复
2,087 次查看
Ruban1
Contributor II

Thank you

0 项奖励
回复
2,110 次查看
Ruban1
Contributor II

Path from which i have to open the terminal and RUN the command

0 项奖励
回复