how to flash custom scfw image in IMX8QXP using JTAG ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to flash custom scfw image in IMX8QXP using JTAG ?

748 Views
krunaldhonde
Contributor I

 

We are having custom board similar to IMX8QXP in which we are not having usb type c and SD card slot.

We want to flash custom scfw image into board using JTAG. We have used following link to generate scfw image. Does this link is correct ?

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

How to flash generated SCFW image using JTAG ?

0 Kudos
Reply
1 Reply

736 Views
igorpadykov
NXP Employee
NXP Employee

Hi Krunal

 

>We have used following link to generate scfw image. Does this link is correct ?

 

yes

 

>How to flash generated SCFW image using JTAG ?

 

I am afraid it is not possible. For for writing flash.bin (SCFW image) to SD one can
follow sect.6.1 Run an example application on the M4 core Getting Started with MCUXpresso

SDK for MEK-MIMX8QX.pdf included in SDK_MEK-MIMX8QX package available on  https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor