how to flash android demo image to SD card through a CARD READER -

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to flash android demo image to SD card through a CARD READER -

800 次查看
Tooght
Contributor III

Hi,

I need to flash an android demo image(currently available android-13.0.0_1.0.0_image) to an sd card. But the thing is I do not have usb connection with the board. So, I am wondering if it is possible to flash the sd card through a usb card reader instead of flashing the sd card on the dev board through usb connection with the board.

I have an i.MX 8M Quad EVK Board 

标记 (3)
0 项奖励
回复
2 回复数

786 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can flash Linux image by card reader but you can't flash Andoird with it. Please connect the USB port.

0 项奖励
回复

778 次查看
Tooght
Contributor III

Hi @Zhiming_Liu, thanks for the quick reply.

I have to do that otherwise I won't be able to use anymore the board. I have a custom board based on 8mq without mmc And booot config doesn't allows me to flash over USB. Please shed me some light how to flash by card reader.

 

0 项奖励
回复