how much current can imx6ull gpio source and sink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how much current can imx6ull gpio source and sink

1,310 次查看
johnmihelic
Contributor I

Can a imx6ull GPIO port at 3.3V drive an LED directly at 10mA

0 项奖励
回复
1 回复

975 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi John,

There is no specific value for a single GPIO current value. It should be calculated considering all the GPIOs currents from NVCC_GPIO rail, as mentioned on Note 5 of Table 13 “Maximum Supply Currents” of i.MX6ULL Datasheet, available at the following link:

http://www.nxp.com/docs/en/data-sheet/IMX6ULLIEC.pdf

You could also take a look at the following Community threads:

https://community.nxp.com/thread/385130

https://community.nxp.com/thread/322294


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复