hdmi gets suspended on imx6q built with prebuilt kitkat

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hdmi gets suspended on imx6q built with prebuilt kitkat

770 Views
amitkulkarni
Contributor II

I have im6q for smart devices on which i have downloaded pre-built kitkat image. Previously console was  freezing approx in 60sec after switching on the board. Solution to that i found was :

echo test > /sys/power/wake_lock

That's solved my console freezing issue.

Now my HDMI monitor is getting suspended. How should i resolve this ?

How can i handle this power management of android ?

Labels (3)
Tags (3)
2 Replies

628 Views
amitkulkarni
Contributor II

okay i set some boot arguments which are given in user guides and solved this.

0 Kudos
Reply

628 Views
SergioSolis
NXP Employee
NXP Employee

Hello Amit, thank you for updating the thread and posting how you solved it.

It is recommended always to go through all the android user guides since there are a lot of instructions and there are cases that by missing just 1 can cause the system to crash.

have a nice day!