Hi,
I would like to resize the video screen to height=400, width=700, x=0, y=40. Please tell me how to do it using the gst-launch.
I tried the following command but did not work for me.
gst-launch playbin2 uri=file://var/youtube.mp4 video-sink='mfw_isink disp-width=700 disp-height=400 axis-top=40 axis-left=0'
Please help.
Regards,
Swamy
已解决! 转到解答。
Sorry for delay.
I tried to figure out if there is any missing framebuffer configuration but I was not able to find it.
I would suggest you to dig into mfw_v4lsink (or even mfw_isink) in order to see if there is any piece of code that would resize only one frame buffer.
For example, if mfw_v4lsink resize only fb0 and it´s hardcoded, and you use fb1. So needs to change it.
I hope someone else can point you a better approach.
Sorry for delay.
I tried to figure out if there is any missing framebuffer configuration but I was not able to find it.
I would suggest you to dig into mfw_v4lsink (or even mfw_isink) in order to see if there is any piece of code that would resize only one frame buffer.
For example, if mfw_v4lsink resize only fb0 and it´s hardcoded, and you use fb1. So needs to change it.
I hope someone else can point you a better approach.
Yes, Even I copied the gplay binary and its related library built on customized IMX535 board to the IMX53QSB and it found to be working as shown by you.
But somehow the same stuff is not working in the custom board, it is resizing to 800x480...Is it because of the video or fb0 needs to be reconfigured somewhere else in the code to suit the changes?
Regards
Swamy
static struct fb_videomode video_modes[] = {
/* NTSC TV output */
"TV-NTSC", 60, 720, 480, 74074,
122, 15,
18, 26,
1, 1,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT | FB_SYNC_EXT,
FB_VMODE_INTERLACED,
0,},
{
/* PAL TV output */
"TV-PAL", 50, 720, 576, 74074,
132, 11,
22, 26,
1, 1,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT | FB_SYNC_EXT,
FB_VMODE_INTERLACED | FB_VMODE_ODD_FLD_FIRST,
0,},
{
"720P60", 60, 1280, 720, 13468,
260, 109,
25, 4,
1, 1,
FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT |
FB_SYNC_EXT, |
FB_VMODE_NONINTERLACED,
0,},
{
/* 800x480 @ 57 Hz , pixel clk @ 27MHz */
"CLAA-WVGA", 57, 800, 480, 37037, 40, 60, 10, 10, 20, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},
{
/* 1600x1200 @ 60 Hz 162M pixel clk*/
"UXGA", 60, 1600, 1200, 6172,
304, 64,
1, 46,
192, 3,
FB_SYNC_HOR_HIGH_ACT|FB_SYNC_VERT_HIGH_ACT |
FB_SYNC_EXT,
FB_VMODE_NONINTERLACED,
0,},
{
"1080P60", 60, 1920, 1080, 7692,
100, 40,
30, 3,
10, 2,
FB_SYNC_EXT,
FB_VMODE_NONINTERLACED,
0,},
{
"XGA", 60, 1024, 768, 15385,
220, 40,
21, 7,
60, 10,
FB_SYNC_EXT,
FB_VMODE_NONINTERLACED,
0,},
{
/* refresh,xres,yres,pixclock=1^12/33.2MHz,left_margin,right_margin,upper_margin,lower_margin,hsync_len,vsync_len,sync,vmode,flag */ | |
"MY_DIS", 60, 800, 480, 30120, | |
88, 40, | |
31, 10, | |
128, 4, | |
FB_SYNC_EXT, | |
FB_VMODE_NONINTERLACED, | |
0,}, |
};
The last one "MY_DIS" is my configuration..
My display size is 800x480(Main screen), when I click on the video I should display it with this configuration...height=400, width=700, x=0, y=40.
Regards
Swamy
Did you find a solution to this problem ?
I am trying to resize to 320, 240 using this command
gst-launch v4l2src ! 'capture-height=240 capture-width=320' ! mfw_v4lsink
and its displaying on the full screen.
mfw_v4lsink default is full screen.
Please gst-inspect mfw_v4lsink in order to see how to control display size.
(and take a look on the command line I placed here: https://community.freescale.com/message/300759#300759)
This is my gst-inspect element properties output
Element Properties:
name : The name of the object
flags: readable, writable
String. Default: null Current: "mfw_gst_v4lsink_info_t0"
preroll-queue-len : Number of buffers to queue during preroll
flags: readable, writable
Unsigned Integer. Range: 0 - 4294967295 Default: 0 Current: 0
sync : Sync on the clock
flags: readable, writable
Boolean. Default: true Current: true
max-lateness : Maximum number of nanoseconds that a buffer can be late before it is dropped (-1 unlimited)
flags: readable, writable
Integer64. Range: -1 - 9223372036854775807 Default: -1 Current: 20000000
qos : Generate Quality-of-Service events upstream
flags: readable, writable
Boolean. Default: false Current: true
async : Go asynchronously to PAUSED
flags: readable, writable
Boolean. Default: true Current: true
ts-offset : Timestamp offset in nanoseconds
flags: readable, writable
Integer64. Range: -9223372036854775808 - 9223372036854775807 Default: 0 Current: 0
last-buffer : The last buffer received in the sink
flags: readable
MiniObject of type "GstBuffer"
blocksize : Size in bytes to pull per buffer (0 = default)
flags: readable, writable
Unsigned Integer. Range: 0 - 4294967295 Default: 4096 Current: 4096
render-delay : Additional render delay of the sink in nanoseconds
flags: readable, writable
Unsigned Integer64. Range: 0 - -1 Default: 0 Current: 0
show-preroll-frame : Whether to render video frames during preroll
flags: readable, writable
Boolean. Default: true Current: true
disp-width : gets the width of the image to be displayed
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
disp-height : gets the height of the image to be displayed
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
axis-top : gets the top co-ordinate of the origin of display
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
axis-left : gets the left co-ordinate of the origin of display
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
rotate : gets the angle at which display is to be rotated
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
crop-left-by-pixel : set the input image cropping in the left (width)
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
crop-right-by-pixel : set the input image cropping in the right (width)
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
crop-top-by-pixel : set the input image cropping in the top (height)
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
crop-bottom-by-pixel: set the input image cropping in the bottom (height)
flags: readable, writable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
tv-out : set output to TV-OUT
flags: readable, writable
Boolean. Default: false Current: false
tv-mode : set mode to TV-OUT, 0: NTSC, 1: PAL, 2: 720p
flags: readable, writable
Integer. Range: 0 - 2 Default: 0 Current: 3
dump-location : Location of the file to write cropped video YUV stream.Enable it will output image to file instead of V4L device
flags: readable, writable
String. Default: null Current: null
setpara : set parameter of V4L2, 1: Set V4L 2: Set Color
flags: readable, writable
Integer. Range: 0 - 3 Default: 0 Current: 0
force-aspect-ratio : Force Aspect Ratio
flags: readable, writable
Boolean. Default: false Current: false
rendered : Get the total rendered frames
flags: readable
Integer. Range: 0 - 2147483647 Default: 0 Current: 0
[1;32m[--->FINALIZE v4l_sink
I tried the command
gst-launch v4l2src ! mfw_v4lsink disp-width=320 disp-height=240
but my image still displays on full screen 800 *480
can you give me an example how i should edit the command to resize the image to 320*240
and also how should i use the crop elements, because when i try crop-top-by-pixel=240 i get an error in the pipeline
Please, try using the latest BSP.
If you are still not able to make get it working, please, start a new discussion (I think this one is starting to get messed)
If you fell like you can mention me or share it to me.
Thanks
Yes , this worked, I resorted to this after spending a lot of time with mfw_v4lsink.
I can continue my work , with isink so its ok. But for information sake, is the v4lsink not resizing because of a bug in the old bsp. I am using L2.6.35_11.09.01_ER_source
I tried to edit the plugin but failed to do so.
I used the following command line (11.09 BSP + mx53QSB) and I was able to resize and determinate where video area starts.
gst-launch playbin2 uri=file:///home/Ice_Age_Test_Video.mp4 video-sink="mfw_v4lsink disp-width=700 disp-height=400 axis-top=100 axis-left=100"
I am not using QSB. I am using IMX536 but it is customized to our project. The following will play the video but will not resize the video. Is something wrong in the command?
This is my output:
$ gst-launch filesrc location=/var/youtube.mp4 ! qtdemux ! queue max-size-time=0 ! mfw_vpudecoder ! mfw_v4lsink disp-width=700 disp-height=300
(gst-plugin-scanner:585): GLib-GObject-WARNING **: cannot register existing type `GstRTPMux'
(gst-plugin-scanner:585): GStreamer-CRITICAL **: gst_element_register: assertion `g_type_is_a (type, GST_TYPE_ELEMENT)' failed
(gst-plugin-scanner:585): GLib-GObject-WARNING **: cannot register existing type `GstRtpSsrcDemux'
(gst-plugin-scanner:585): GLib-CRITICAL **: g_once_init_leave: assertion `initialization_value != 0' failed
(gst-plugin-scanner:585): GStreamer-CRITICAL **: gst_element_register: assertion `g_type_is_a (type, GST_TYPE_ELEMENT)' failed
MFW_GST_V4LSINK_PLUGIN 2.0.3 build on Sep 13 2012 15:59:37.
Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX53
VPU Version: firmware 13.4.0; libvpu: 5.1.4
MFW_GST_VPU_DECODER_PLUGIN 2.0.3 build on Sep 13 2012 12:44:14.
Pipeline is PREROLLING ...
>>V4L_SINK: Actually buffer status:
hardware buffer : 9
software buffer : 0
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
full screen size:800x480
[V4L Update Display]: left=0, top=0, width=696, height=296
New clock: GstSystemClock
^CCaught interrupt -- handling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 6011361075 ns.
Setting pipeline to PAUSED ...
total time:0:00:06.013819574 ,Render fps:29
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total rendered:180
>>VPU_DEC: State: Ready to Null
Freeing pipeline ...
[--->FINALIZE v4l_sink
[--->FINALIZE vpu_dec