fsl-image-gui has no GUI on iMX 6UL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fsl-image-gui has no GUI on iMX 6UL?

4,234 次查看
kanimozhi_t
Contributor V

Hi,

    We've built the Yocto warrior for iMX 6UL in 'fsl-image-gui' configuration which by definition form 'Freescale Yocto Project User's Guide' is expected to build a "Freescale image with a GUI without any Qt content" but what we seen is a terminal console (image attached) similar to the one produced by 'core-image-full-cmdline'. The only difference is that 'fsl-image-gui' shows a OpenEmbedded splash screen while booting on the connected LCD8000-43T.

    It'll be very helpful if someone could point out the issue, or the steps needed to be followed to get a proper GUI.

Thanks in advance.

2 回复数

4,164 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The i.MX6UL do not have GPU, you can try this https://community.nxp.com/docs/DOC-333580 

4,164 次查看
karangajjar
Senior Contributor II

Hi Kanimozhi Thangappan ,

The default image build for imx6ULL with GUI has matchbox utility to display the various applications on GUI. The default application that runs is console, which is you see Linux console on LCD. You can play video and run the GUI application which will be displayed on the LCD.

You can also try to add QT to build QT applications and display on LCD as suggested by Rita in the above comment.

Regards,

Karan Gajjar