Hi Jorge!
I atached my schematic for your review! Thanks a lot for your time!
Because our custom board has in validation phase yet, we mount only:
imx28-pmu(page 1), imx28-psu/emi-bus (page 2), imx28-lcd_bus/gpmi (page 3)
imx28-ethernet/pwm/saif/usb/adc (page 4), imx28-spi-uart-can-i2c (page 5),
nand-flash (page 7), ddr2 (page 8), SSP-interface (page 11),
uart-interface (page 12), power-supply (page 23).
Note that we already made some changes in the schematics (but not update the document yet):
1). The PSWITCH and RESET circuit is now the same found in the MX28 EVK
2). I remove the C38 from my board (can be found in page 01)
3). The net PWRGATE_SSP0 found in the page 05 (imx28 pin D2) has connected now
into the PWM3/GPIO3_28 (imx28 pin E9) -- This pin enable the power-supply
of the MMC Card.
4). I changed the debug uart pins (nets uP_DUART_RX and uP_DUART_TX -- imx28 pins C7 and D8)
to imx28 pins K7 and L7; like found in the MX28 EVK.
5). Change the value of R125 to 470kR like found in the MX28 EVK.
I've already check the boot-loader configuration mode that in my board can be done through
resistors (page 09).
In respect of reproduce the same error on MX28 EVK, the error not
happens and I use the same SD Card with the same "images" (imx-bootlets+linux image).
Thanks,
Christian
Jorge Ramírez Rivero said:
Hi Cristian,
Never seen this problem, but may I offer to help you by checking your schematics for possible issues? Are you able to reproduce it in the MX28 EVK?
Best regards.
Jorge.