can't get kernel image error in imx25 pdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can't get kernel image error in imx25 pdk

ソリューションへジャンプ
3,365件の閲覧回数
arumugamramasam
Contributor II

Hi,

I am using iMX25 PDK with 3 stack configuration. I have reproduced the CPU boards and using with the personality board supplied by freescale. While booting from SD card, the original CPU is booting and one of my newly produced CPUs is also booting. But without changing the SD Card, if I change the CPU, it is not booting up. Saying that can't load kernel image. The log files of good and bad booting are attached. Need help to find the reason why is it malfunctioning between CPU to CPU.

 

Thanks,

Arumugam R

Original Attachment has been moved to: Kernel-Loaded.txt.zip

Original Attachment has been moved to: Can't-get-kernel-image.txt.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
2,871件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Your understand is correct.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,871件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Do you mean you made two identical CPU boards? Then one is good, it can boot up without any problem. The other one cannot boot up, right? According to the log, the bad one the kernel can be loaded to DDR, but it cannot be executed.

Please try to decrease the DDR freq.. Please check the DDR (hardware) soldering on the board.

0 件の賞賛
返信
2,871件の閲覧回数
arumugamramasam
Contributor II

Thanks for the response. But the same board boots from Nand. If in case there is any problem with DDR then it should not have booted from Nand either right? Please let me know whether my understanding is correct or not.

Thanks,

Arumugam R

0 件の賞賛
返信
2,872件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Your understand is correct.

0 件の賞賛
返信