board freeze after indeterminate duration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

board freeze after indeterminate duration

850件の閲覧回数
wolfgangschneid
Contributor I

we have a custom i.mx6d board with android 5.0.2 implementation. after indeterminate duration the board freezes without any debug information on the serial console. we have done RAM calibration with the stress test tool and several memory tests without any error. mtest in bootloader and memtester in kernel with overclocking (580Mhz) an high temperature without error.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

786件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Wolfgang,

    if you want to display booting logs on serical console, you should modify booting parameters of u-boot, add "selinux=disable" to environment of u-boot, then save it and reboot.

Best Regards,

Weidong

0 件の賞賛
返信

786件の閲覧回数
wolfgangschneid
Contributor I

Hello Weidong,

we have already done this. see the copy from the console.

        enable_wait_mode=off console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.selinux=disabled androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M vt.global_cursor_default=0 enable_wait_mode=off

we can't search for a mistake because the system tells us nothing !

do you have another idea ?

0 件の賞賛
返信

786件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Wolfgang,

      Can android successfully boot? For example, android GUI is normally displayed on screen.

Regards,

Weidong

0 件の賞賛
返信